Dust Collection Filters, BHA Knows Dust Collection - Industrial Gas Filtration & Generation Division | Parker US
Parker Image

Our filtration and baghouse experts work with you to find the right dust collection filters to positively impact the performance and reliability of your baghouse and dust collection equipment.

24/7 Support

We answer your baghouse and dust collection filter needs. We are here to offer support for your BHA filters 24/7. Call us at +1 (800) 821-2222 or +1 (913) 374-3300. We are here to help.

High Efficiency Baghouse Filtration

Improve Efficiency and Airflow in Your Baghouse

You have much to consider when selecting bag house filters, what media suits your application, the filter style, and size. Rely on BHA products from Parker. We have been doing this for half a century. We have helped managers of baghouses improve dust collection, troubleshoot problems, and improve maintenance. Watch this smoke test video to see how Preveil® ePTFE membrane stops fine particulate, giving you lower energy costs and longer filter life.

High Efficiency Baghouse Filtration

EnviroSeam™

Our new proprietary technology, EnviroSeam™, ensures consistent performance and mitigates leaks that are common in most laminated filter bags. Don’t just take our word for it, look at the test results!

Parker Image

BHA Pleated Cartridge Dust Collection Filters

At Parker Hannifin, when it comes to industrial, dust cartridge filters we’re known for delivering filters that provide higher efficiencies with cleaner air, longer filter life, and greater energy savings. We are at the forefront of technology and innovation; we develop and manufacture proprietary filter media technologies using our advanced research capabilities to ensure the latest developments are in our filters. Our products are also performance certified by 3rd party testing services, and you can trust our products will perform reliably.

Our application and technical experts are here to help you work through the MERV rating that is right for your application and operating conditions. We have a vast selection of patented media to choose from and we will help ensure the media you use will minimize energy consumption and compressed air usage.

BHA Pleated Cartridge Dust Collection Filters

BHA Preveil® EPTFE Membrane Filters

BHA Preveil membrane bag house filters are made with a microporous ePTFE (expanded polytetrafluoroethylene) membrane bonded to conventional filter media's surface, including felts and woven fabrics, to provide one of the highest efficiencies of any available filter bag media.

Preveil is made from PTFE resin, a substance with inherent non-stick properties that can be used to help your dust collector operate at maximum efficiency by providing the following:

  • 99.99% efficiency
  • Higher airflow
  • Better cleaning


One of only a handful of organizations globally, we offer testing capability ASTM D6830-02 and VDI/DIN-3926. PTFE membrane filter media selection is one of the most critical factors in optimizing fabric filter performance in your baghouse, and testing helps ensure quality. For added peace of mind, we offer performance guarantees on select BHA Preveil laminated baghouse filter bags for qualified applications.

An independent laboratory performed a Variable Environmental Simulation Analysis to determine the efficiencies of two membrane fabrics. Check the results to see where Preveil outperformed in emissions control, differential pressure, and efficiency.

BHA Baghouse Filters and Cages

We deliver reliable and durable baghouse fabric filters and cages engineered to meet the needs of your unique systems. Parker can deliver almost any filter for your baghouse, regardless of OEM design and system conditions. Because of the variety of particulates collected and individual operational conditions of collection systems, the selection of replacement filters should be determined by carefully analyzing your current operating parameters. Our filtration specialists ensure the baghouse filters are optimized for your application.

We also have support cages available in various sizes, wire configurations, and materials to ensure optimum performance in unison with the proper fabric.

BHA Baghouse Filters and Cages

Industrial Filter Test Lab

The Industrial Filter Test Lab allows our engineers to conduct precise media and filter testing in the development of innovative filtration technologies. The highlight of the lab is a test rig dedicated to testing in accordance with ANSI/ASHRAE 199-2016 which provides a quantitative method for determining the performance of pulse cleaned filters.

 

As a leading global provider of innovative filtration technologies and solutions, creating the Filter Test Lab and Customer Experience Facility is essential to finding the answers for our customer's biggest challenges.

The Industrial Filter Test Lab allows our engineers to conduct precise media and filter testing in the development of innovative filtration technologies. The highlight of the lab is a test rig dedicated to testing in accordance with ANSI/ASHRAE 199-2016. The test rig provides a quantitative method for determining the performance of pulse cleaned filters. The unit feeds dust through a humidity and temperature controlled loop, then into a dust collector with instrumentation that measures differential pressure and fractional efficiency. The rig is used in the design, construction, and selection of new filter technology. As a leading global provider of innovative filtration technologies and solutions, creating the Filter Test Lab and Customer Experience Facility is essential to finding the answers to our customer’s biggest challenges.The Industrial Filter Test Lab is available for tours during visits as well as during our customer seminars. Customers will observe the various testing methods conducted across flat media, pleated filtration, finished filter testing methods, and competitive testing.

BHA Dust Collection Filters FAQ

Q: What is the best material to filter industrial dust?

The best material for an industrial dust filter depends on the type of dust being collected, the operating conditions, and the specific requirements of your dust collection system.  

  • Polyester is a popular choice for dust filter bags because it is durable, affordable, and has good resistance to most mineral acids and oxidizing agents. It is a versatile material that can handle a wide range of dust types and conditions.

  • Aramid fibers, often known by the brand name Nomex, are extremely heat-resistant, making them ideal for high-temperature applications.
    They also offer excellent resistance to abrasion and most mineral acids.

  • Polypropylene is a cost-effective choice that offers good resistance to most acids and alkalis. It also has excellent moisture resistance, making it a good choice for applications with high humidity.

  • PTFE, often known by the brand name Teflon, is highly resistant to most chemicals and high temperatures. It also has excellent moisture resistance. However, it is more expensive than other materials.

  • Fiberglass filters are often used in high-temperature applications. They offer good resistance to most chemicals but can be more prone to abrasion.

  • Ryton, or polyphenylene sulfide (PPS), is a material that offers excellent chemical resistance and can withstand high temperatures. It is often used in applications where harsh chemicals are present. 

In addition to the base material, many filters also have finishes or treatments to enhance their performance. Our Preveil® membrane, a proprietary technology is added to improve efficiency. Some treatments are oleophobic and repel oil and water. There's no one-size-fits-all answer to this question. The best material for your dust filter depends on your specific needs and circumstances. 

Q: How often should I change my dust collector filter?

The frequency at which you should change your dust collector filter depends on several factors, including the type of dust, the volume of dust, the type of filter, and the specific design of your dust collection system. 

  • Check Pressure Drop: A common way to determine when a filter needs to be replaced is by monitoring the pressure drop across the filter. As the filter collects dust, it becomes more difficult for air to pass through it, causing a pressure drop. When the pressure drop reaches a certain point, it is time to replace the filter. The specific pressure drop that indicates a need for replacement will depend on your system and the type of filter you are using.

  • Visual Inspection and Manual Checks: Regularly inspect your filters for signs of wear or damage, such as holes or tears. Also, check for dust breakthrough or any changes in the operation of your dust collector, such as increased noise or decreased suction, which may indicate a need for filter replacement.

  • Scheduled Maintenance: Some operations choose to replace their filters on a regular schedule, such as every six months or every year, to ensure optimal performance. However, this approach may not be the most cost-effective if your filters still have useful life left.

  • Manufacturer's Recommendations: Always refer to the manufacturer's guidelines for filter replacement. They will provide specific recommendations based on the type of filter and its intended use. 

In addition to the base material, many filters also have finishes or treatments to enhance their performance. Our Preveil® membrane, a proprietary technology is added to improve efficiency. Some treatments are oleophobic and repel oil and water. There's no one-size-fits-all answer to this question. The best material for your dust filter depends on your specific needs and circumstances. 

Q: How much CFM do I need for dust collection?

The amount of Cubic Feet per Minute (CFM) you need for dust collection is dependent on the type of machines you are using, the size of your workspace, and the number of machines running simultaneously. The specific CFM requirement for your situation may vary.  

  • Each type of machine has a recommended CFM for effective dust collection. You can often find these recommendations in the machine's user manual or from the manufacturer.

  • If you are running multiple machines at the same time, you'll need to add up the CFM requirements for each machine. However, if you are only using one machine at a time, you might only need to meet the CFM requirement for the machine with the highest CFM need.

  • The layout of your dust collection system can also affect the CFM requirement. Long runs of ductwork, bends in the ductwork, and vertical ducts can all increase the amount of CFM needed.

  • The efficiency of your dust collector and filter can also impact the CFM requirement. A more efficient system may be able to handle the same amount of dust with less CFM.

  • Larger spaces may require a higher CFM to effectively control dust, especially if the dust is being dispersed throughout the room. 

Q: What filter is best for dust?

The best filter for dust depends on the type of dust and the specific requirements of your dust collection system.  

  • Baghouse Filters: Baghouse filters, also known as bag filters, are commonly used in dust collection systems. They consist of a large bag made of fabric or other material that collects dust on its surface. The dust is then shaken or blasted off the bag for disposal.

  • Cartridge Filters are compact, cylindrical filters that offer a large surface area for dust collection. They are often used in smaller, portable dust collectors and are typically easy to replace.

  • Pleated Filters, or PulsePleat® filters have a series of folds that increase the surface area of the filter, allowing it to capture more dust The cost is generally a little higher, but the return on investment makes it an affordable choice.

  • HEPA (High Efficiency Particulate Air) Filters are able to capture 99.97% of particles that are 0.3 microns or larger, making them extremely efficient at dust collection. However, they also require more energy to push air through, so they may not be suitable for all applications.

  • PTFE (polytetrafluoroethylene, often known by the brand name Teflon) Membrane Filters have a high dust release quality, which makes them a good choice for dust collection systems that use pulse-jet cleaning. 

BHA Powerwave® Acoustic and Impulse Cleaning Systems

Our Powerwave+ acoustic cleaning system significantly improves the cleaning of air pollution control equipment, heat transfer surfaces, material handling and storage equipment, and areas of production where particulate buildup occurs. As an alternative to soot blowers and soot blower cleaning, acoustic cleaners are air-operated devices that emit low-frequency, high-energy sound waves. The sound waves create vibrations powerful enough to break apart and dislodge heavy concentrations of particulate on surfaces, but gentle enough to not harm the surface.

The BHA Powerwave+ impulse cleaning system enhances boiler operation and minimizes high maintenance expenses associated with other cleaning methods. This technology provides advantages over traditional methods. 


Advantages of Our Acoustic Cleaning System:

  • Powerful online cleaning technology that removes ash deposits better 
  • Reduces the need for steam soot blowing
  • Enhances long-term operational ability
  • Safer - doesn't require personnel to enter the area where buildup occurs
  • Fuel-efficient design has a low operating cost with minimal maintenance
  • Increases heat transfer and overall efficiency of processes
  • Extends time intervals between downturns caused by off-line cleaning, allowing more time for production
  • Easy to install and maintain, with a small footprint that preserves valuable space