How to Install - Fluid System Connectors Division | Parker US
Transair Installation Resources

Transair compressed air piping installs fast and with minimal tooling and no specialized labor. Parker Hannifin is dedicated to your success in installing a Transair system. Browse our content below for installation how to guides and videos.

Transair Piping Install Manual

Transair aluminum and stainless steel piping installs fast with minimal tooling and no specialized labor. The lightweight materials make maneuvering and install compressed air piping in the air much easier. than heavy black iron. On average, a Transair compressed air piping system can be installed 4x faster than traditionally materials such as copper or steel. For proper installation techniques, download our installation manual. Our manual will provide everything you need to know to properly install a Transair aluminum or stainless steel piping system. 

Transair Piping Install Manual

TCM Install Manual

Transair Condition Monitoring provides alerts and data to monitor and analyze the health of your compressed air system. Our wireless sensors communicate to a cloud-based website via a collection server. All TCM sensors come from the factory joined to the collection server. All you need to do is install the sensors in your compressed air piping system based on the locations identified in your site survey. 

For installation assistance, please contact your local Transair representative. 

TCM Install Manual

Aluminum Pipe Installation

Transair is the original, lightweight, and easy to install aluminum piping system. Transair aluminum piping can be used for compressed air, vacuum, and industrial / inert gas piping applications. All piping arrives from the factory ready to install and features a durable coating to provide years of dependable service in challenging environments. If a pipe needs to be cut to fit the installation area, follow the applicable instructions for the diameter to ensure the aluminum pipe is properly prepared to accept the fittings. For a quick review of how to install Transair compressed air piping, watch our videos below! 

Drop Bracket Installation

Transair drop brackets allow for a quick and easy way to run compressed air piping from the distribution piping to the point of use. Installing a Transair compressed air drop line only takes about seven minutes! Parker Transair offers multiple styles of brackets to ensure we have one that will fit your application. Installing a drop bracket is fast and easy. Watch our installation video to learn how to install a drop bracket in an existing Transair compressed air piping system. Please note: Transair drop brackets can only be installed when no compressed air is present in the pipe. 

This video demonstrates the assembly procedures for installing a drop bracket in an existing line.

Hot Tap Bracket Installation

For instances where a pressurized compressed air pipe cannot be depressurized, Parker Transair offers the hot tap/pressurized system bracket for installing a drop on a live system. The bracket has a ball valve so after drilling the hole into the live pipe, the flow of air can be shut-off while the rest of the compressed air drop is assembled. Installing a Transair hot tap bracket requires a special drilling tool.


To learn how to install the Transair hot tap bracket, watch the video. Please note: Compressed air can be very dangerous if not respected, always wear proper PPE when installing a hot tap bracket. 

The Transair hot tap bracket can be installed on a pressurized Transair compressed air piping system. Follow all safety precautions and watch the video to learn how to install the hot tap bracket.

Drilling Holes in Transair Piping

A Transair aluminum or stainless steel piping system can easily be modified 4x faster than traditional piping methods such as copper or black iron. With the proper Transair tools, a drop line can be added to an existing Transair compressed air piping system in just 7 minutes! To accomplish the task of drilling holes in Transair piping, Parker Transair offers a series of tools and procedure steps to make the task easier. Watch our videos below to help select the correct drill bit and learn how to drill holes in Transair aluminum or stainless steel compressed air piping. 


Selecting the Correct Drill Bit
: To make the job of drilling Transair compressed air piping easier, Parker Transair offers a series of drilling tools. Sometimes, selecting the correct drill bit for the application can be a challenge. This video will simplify the drill bit selection process.

Transair offers a few different drill bits for use in drilling holes in Transair aluminum pipe. This video breaks down each bit and shows which bit is needed to install which drop bracket.

Have a question?

Are you designing or installing an aluminum compressed air piping system and have technical questions? Parker Transair has experienced representatives dedicated to helping answer your questions. Our representatives can assist with system design and technical details for your next aluminum compressed air piping system. In addition to our technical representatives, Parker Transair has established a network of local service providers and distribution centers to ensure our customers get the assistance and products they need in a timely fashion. Contact us to find your local representative!