Pressurized metered dose inhalers (pMDI’s) have long been a safe and effective means of delivering inhaled pharmaceuticals for the treatment of asthma and other respiratory ailments. MDI’s were originally developed to use the propellant P-12, dichlorodifluoromethane. However, with the recognition that CFC propellants were a significant contributor to the depletion of ozone in the upper atmosphere, the use of P-12 was phased out, being replaced with 1,1,1,2-tetrafluoroethane, also known as P-134a.
The industry is now looking to make another wholesale change to the propellants used in metered dose inhalers for a number of reasons. First and foremost, P-134a has a relatively high Global Warming Potential (GWP) of 1,300. While the amount of propellant released over the life of a metered dose inhaler is quite small compared to that present in a refrigeration system or a non-medicinal aerosol, the number of inhalers used globally over the course of year result in a meaningful amount of propellant entering the atmosphere. In addition, P-134a meets the technical definition of perfluorinated alkyl substance (PFAS) due to the presence of carbon atom bonded to three fluorine atoms. With the regulatory attention being given to all such substances, it may be time for the industry to move away from P-134a.
The two leading candidates for a next-generation propellant appear to be difluoroethane (P-152a) and trans-1,3,3,3-tetrafluoropropene (P-1234ze.) Both propellants have pros and cons to consider when replacing P-134a, and these impact seal material selection when sealing the different propellants.
P-1234ze has many things going for it, but it’s certainly not perfect. In terms of seal material compatibility, extensive testing has already been done with its nearly identical twin, R-1234yf. The automotive industry has already made the switch in mobile air conditioning from R-134a to R-1234yf. The ethylene-propylene (EPDM) and acrylonitrile-butadiene (NBR and HNBR) seal materials that have been used for years in R-134a applications function just as well in R-1234yf. It is not a leap to expect the same similarity of performance with the EPDM and NBR seal materials that have long been used in pMDI’s. Because it is a larger molecule than P-134a, P-1234ze also exhibits less permeation through seal materials over time. P-1234 also has zero ozone depletion potential and a GWP of less than 1 (less than carbon dioxide.) However, it is designed to decompose in the environment, and one of the potential decomposition products has a GWP of almost 15,000. Another decomposition product is trifluoroacetate, which can contaminate ground water and is very difficult to remove once dissolved. Even though P-1234ze is technically an olefin, meaning it has at least one carbon-carbon double bond, and not an alkane, it is still classified as a perfluorinated alkyl substance (PFAS) under some regulations.
In addition to being extremely flammable, it is also an intoxicant. While the exposure from proper use of a pMDI is well below the published toxicity levels, there have been documented fatalities related to intentional abuse. The GWP of P-152a is reasonably low 124, and it is not classified as a PFAS, so it is unlikely to be impacted by PFAS legislation. From a seal compatibility standpoint, P-152a is noticeably more able to permeate through most seal materials than P-134a. With EPDM, permeation loss over long periods of time could impact the shelf life of an assembled pMDI. Parker’s existing pMDI EPDM and NBR materials may still be acceptable in a P-152 pMDI application, but this gradual loss of propellant should be evaluated for a particular application.
Parker is also developing a next-generation low permeation material specifically for P-152a pMDI’s based on butyl rubber technology. Butyl rubber is well-known for having extremely low permeation with small gaseous molecules, and compatibility with other substances is very similar to that of EPDM. Mechanically, butyl rubber behaves much differently than EPDM and NBR. In addition to low permeation, Parker’s development work focuses on minimizing the extractible content from the finished rubber material, and specifically the elimination of potentially toxic byproducts of the cure reaction, as well as the elimination of pigments.
For more information on Parker’s drug delivery devices visit us online or contact us directly at oesmailbox@parker.com (859-335-5101).
Senior Chemist
O-Ring & Engineered Seals Division
Webinar
Advanced Sealing Solutions for Longevity & Sustainability
Are you facing sealing challenges in drug delivery device design? Join Parker O-Ring & Engineered Seals (OES) for an exclusive webinar tailored to the Life Science market. Discover how precision-engineered sealing solutions can enhance reliability, longevity, and sustainability in your projects. Learn about advanced sealing technologies designed to meet the unique demands of drug delivery devices while ensuring regulatory compliance. Don’t miss this opportunity to gain actionable insights that will accelerate your time to market and elevate your device designs.
Key Takeaways:
Insights into Parker OES’s cutting-edge design and manufacturing excellence
Overview of molded sealing solutions including micro O-rings, custom shapes, and overmolded seals
Understanding extrusion and splicing techniques for versatile sealing options
Introduction to innovative seal materials certified to ISO 10993 and USP Class VI
Strategies to improve device performance and regulatory compliance