How to Ground Electronics

A global defense contractor is tasked with developing the next generation of armored land fighting vehicles, each needing to provide first-class protection and survivability, reliability and all-weather performance.

Armored vehicles are now being designed and developed with IoMT (Internet of Military Things) in mind, compassing a large range off intelligent sensing, learning, and actuation capabilities through virtual or cyber interfaces that are integrated into the vehicle’s systems.

EMI Shielding and Sealing Challenges

All on board electronics need to work efficiently and reliably, but due to the complexity of the operating systems and the volume of electronics inside the vehicle, electromagnetic interference (EMI) is a large issue for the customer. 

Both an EMI solution and environmental weather sealing is required around the ingress and egress hatches to prevent rainwater/fluid from entering the vehicle. 

Multiple optical periscope cameras and sensors on the vehicle required EMI/RFI shielding to ensure reliability. All air intake and exhaust ducts required EMI shielded ventilation panels to allow for airflow but shield extraneous RF waves.

MIL-STD Design Requirements for EMI Shielding

The armored fighting vehicle needed to become essentially an armored Faraday cage to protect the internal electronics to ensure their smooth and reliable operation in the battlefield. We've written extensively about EMI shielding technology necessary for defense applications on our blog.

EMI shielding materials need to meet rigorous military standards (MIL-STD) and are subject to stringent EMI testing. EMI/RFI signature from the vehicle needs to be reduced to prevent the vehicle being picked up by enemy tracking systems.   

Key Program Requirements

Both EMI shielding and corrosion resistant materials are required. Materials should be resistant to harsh fluids, including chemical washdown.  

Each armored fighting vehicle needs to be ‘future-proofed’ to ensure it can be upgraded quickly and effectively throughout its service. 

Armored personnel type carrier
Parker Image

EMI shielding around touch screen display.

Parker Image

Electrically conductive elastomer gaskets around hatch seals and doors.

To provide an effective EMI and environmental seal to ingress and egress hatches, the following materials are being designed into the application. 

Parker Chomerics application engineers, in partnership with the customer’s design team, determined that CHO-SHIELD 2002, an electrically conductive polyurethane coating with a copper conductive filler would help to aid in corrosion resistance. This material is specifically formulated to offer corrosion protection for enclosure flanges which mate with EMI shielding gaskets. It also offers excellent chemical resistance to hydraulic fluids and motor oils. 

To help fill seams in gaps and around rivets, a silver-plated aluminum filled silicone electrically conductive sealant called CHO-BOND 1075 was used to give additional EMI protection and to provide an adhesive bond for the gasket. 

A robust dual gasket configuration, called a co-extrusion, made from CHO-SEAL 1298 material, containing both a silver-aluminum filled electrically conductive silicone gasket alongside a non-conductive military grade environmental gasket was also chosen. This gasket was positioned around the entrance hatches to ensure compliance with both EMI and environmental requirements.  

In other applications on the vehicle, CHO-SEAL 1298 EMI shielding gaskets were custom made for use with multiple periscopes cameras. Several connector gaskets were also fabricated out of CHO-SEAL 1298 material and were used to shield electronic hardware. 

 

All air intake and exhaust ducts required circular steel EMI honeycomb vents, fitted to allow air flow while providing an EMI shield. 

 

The Parker Chomerics applications engineering team worked closely with the customer design team to meet rigorous testing procedures and ensure compliance of all specified technologies.  

Parker Image

Get a Quote Now

Tell us a little bit about your problem and we'll do our best to come up with a cost effective, timely quote to help you get started.

Need Help Finding the Right Solution? Talk to an Expert Engineer Now.

If you need assistance identifying the most suitable product for your application,  speak with one of our expert engineers. Our team is ready to help.

Learn more about high-performing EMI shielding solutions.

EMI Shielding Technology Applications in Defense Systems

As the defense industry continues to push the boundaries on advanced electronic systems and state-of-the-art communication devices, the requirements governing these programs must follow suit. Among the many technical requirements is Electromagnetic Compatibility, defined as the ability of a device to withstand both anticipated and unanticipated electronic interference (EMI) as well as minimize the interference being radiated.

Parker Image

Solutions for Thermal Interface Materials

Parker Chomerics thermal interface materials transfer heat from electronic components to heat sinks and are used to eliminate air gaps from the interface. Our THERM-A-GAP® materials deliver lower thermal impedance, higher thermal conductivity and greater compliance and conformability to both microelectronics and large scale electronics.

Blog: Thermal Gels or Gap Filler Pads? Top 6 Things You Should Know

Our products are used in a wide range of industries.


 

Thermal Interface Materials & EMI Shielding Solutions

With more than 60 years of experience, we have the technical know-how to meet the rapidly increasing needs of engineers.

Can't find what you're looking for? Talk to one of our experts.