Custom Plan Views - O-Ring & Engineered Seals Division | Parker US

Custom Plan Views

O-rings are successfully used in rectangular or non-circular groove patterns as long as the groove design follows a few basic principles.

 

A non-circular face seal footprint might also be called a race track groove, a wandering groove or a custom plan view. When using a seal with a round inner diameter and a round cross section will work. The main design consideration is the corner or smallest radius the seal must bend around. The inside radius should be at three times the O-ring cross sectional diameter. In a perfect world, six times greater is even better.

 

What we want to avoid is over-stressing the O-ring around the bend, or causing a corner crease which increases likelihood of corner leakage. Designing the radius at six times the cross section will minimize the bending stress, resulting in increased service life.

Custom Plan Views

Questions? Send us a message and let us know how we can help!