O-Ring Elastomers - O-Ring & Engineered Seals Division | Parker US
Parker Image

Elastomers used in producing seals, and particularly those used in O-rings, will usually provide reliable, leak-free function if fundamental design requirements are observed.. Learn more about the characteristics and materials of elastomers.

Overview

The basic core polymer of an elastomeric compound is called a rubber, produced either as natural gum rubber or manufactured synthetically by the chemical industry. Today, more than 32 synthetic rubbers are known, the most important ones are listed here.

Modern elastomeric sealing compounds generally contain 50 to 60% base polymer and are often described simply as “rubber.” The remaining balance of an elastomeric compound consists of various fillers, vulcanizing agents, accelerators, aging retardants and other chemical additives which modify and improve the basic physical properties of the base polymer to meet the particular requirements of a specific application.

Elastomers used in producing seals, and particularly those used in O-rings, will usually provide reliable, leak-free function if fundamental design requirements are observed.

What exactly makes a rubber compound behave the way it does? The magic is in "cross-linking." Bridges tie together the polymer chains forming bonds during the vulcanization process, as depicted in the image below. Cross-linking of the molecules changes the rubber from a plastic-like material to an elastic material.

 

Elasticity is what allows a rubber compound to function as a seal. When a rubber compound is compressed, the "cross-linked" polymer chains are pushed close together. These cross linked bonds want to extend to their original state acting as springs, pushing the rubber compound outwards. The rubber conforms to the gland surfaces and creates a barrier, preventing fluid from crossing, and thus creating a good seal.

 

Elastomer with no cross-links

 

After vulcanization, including any required “post-cure,” an elastomer compound attains the physical properties required for a good sealing material. As with all chemical reactions, temperature is responsible for the speed of reaction. Only when the ideal process temperature is constant during the entire vulcanization time, will the optimum degree of curing be reached. For this reason, the conditions of vulcanization are closely controlled and recorded as part of the Parker quality assurance process.

Elastomer with cross-links

Concepts & Definitions

Before reviewing the available elastomers and their general properties, it is necessary to fully understand the terms “polymer,” “rubber,” “elastomer” and “compound” as they are used in this ehandbook.

Polymer

A polymer is a compound composed of many smaller molecules which are linked together. Both plastics and elastomers are classified as polymers. In this handbook, polymers generally refer to a basic class of elastomers, members of which have similar chemical and physical properties. O-Rings are made from many polymers, but a few polymers account for the majority of O-Rings produced, namely nitrile (nbr), ethylene propylene (epdm), and polychloroprene (CR).

Rubber

The term rubber can refer to two different types: natural rubber and synthetic rubber. Originally all rubber was manufactured from latex extracted from rubber trees. During the early 20th century, the need arose for other rubber-like materials and synthetic rubber was born. Synthetic rubber is composed of polymers which are derived from chemical processes. Since then, usage in the industry has broadened the meaning of the term “rubber” to include both natural as well as synthetic materials having rubber-like qualities. This handbook uses the broader meaning of the word “rubber.”

 

Elastomer

Though “elastomer” is synonymous with “rubber,” it is formally defined as a “high molecular weight polymer that can be, or has been modified, to a state exhibiting little plastic flow and rapid, nearly complete recovery from an extending or compressing force.” In most instances we call such material before modification “uncured” or “unprocessed” rubber or polymer. When the basic high molecular weight polymer, without the addition of plasticizers or other dilutents, is converted by appropriate means to an essentially non-plastic state and tested at room temperature, it usually meets the following requirements in order to be called an elastomer:

  • It must not break when stretched approximately 100%.
  • After being held for five minutes at 100% stretch, it must retract to within 10% of its original length within five minutes of release.

Note: Extremely high hardness/modulus materials generally do not exhibit these properties even though they are still considered elastomers. The American Society for Testing and Materials (ASTM) uses these criteria to define the term “elastomer.”

 

Compound

A compound is a mixture of base polymer and other chemicals that form a finished rubber material. More precisely, compound refers to a specific blend of chemical ingredients tailored for particular required characteristics to optimize performance in some specific service.

A Parker O-Ring Division rubber chemist begins compound development by selecting a polymer type. There may be a dozen or more different polymer types to choose from depending on the properties required. The rubber chemist may then add various reinforcing agents such as carbon black, curing or vulcanizing agents (such as sulfur or peroxide, activators, plasticizers, accelerators, antioxidants, or antiozonants) to the elastomer mixture to tailor it into a seal compound with its own distinct physical properties. Since Parker chemists have thousands of compounding ingredients at their disposal, it seems reasonable to visualize two, three, or even one hundred-plus compounds having the same base elastomer, yet exhibiting marked performance differences in the O-ring seal.

The terms “compound” and “elastomer” are often used interchangeably in a more general sense. This usage usually references a particular type or class of materials such as “nitrile compounds” or “butyl elastomers.” Please remember that when one specific compound is under discussion in this handbook, it is a blend of various compounding ingredients (including one or more base elastomers) with its own individual characteristics and identification in the form of a unique compound number, For example, N0674-70 or V1164-75.

Physical & Chemical Characteristics

It is important to know the physical and chemical properties and how they interact and affect seal material selection. Learn more about properties including hardness, tensile strength, elongation, permeability and more.

Physical & Chemical Characteristics

Material Selection Guide

This section provides a brief review of the various elastomers currently available for use in Parker's O-rings and custom elastomeric seals. Service recommendations mentioned in this section are necessarily abbreviated.

For more comprehensive and specific information on this important subject, see the Fluid Compatibility Tables in Section VII of the hard print or pdf version of the Parker O-Ring Handbook. Rubber terms described in this section are further explained in the eHandbook glossary. 

Parker Image

Questions? Send us a message and let us know how we can help!