For any company who manufactures or works with electronics, understanding how to reduce electromagnetic interference (EMI) is a chief concern. By becoming more aware of what causes EMI and how to avoid it, companies will be well-positioned to deliver high-performing products that aren’t degraded by the effects of EMI.
EMI is unwanted noise or interference within an electrical circuit. These incidences, which occur as a result of electromagnetic fields from a variety of natural and manmade sources, can impair system performance or even stop it from operating altogether. The potential impacts of EMI become particularly serious and potentially even life-threatening in medical devices such as pacemakers or modern vehicles equipped with advanced driver assistance systems (ADAS). It’s important for producers to consider potential EMI interactions so they can be mitigated before a problem occurs.
If you’re wondering how to avoid electromagnetic interference, the best offense is a good defense. Look at design considerations from multiple angles as early in the process as possible to avoid last-minute modifications, which can add unnecessary expense and delays.
Here are four areas engineers should consider as they investigate how to prevent electromagnetic interference in products and devices:
By having a thorough understanding of a device’s design requirements, companies can choose appropriate products that will mitigate the potential impacts of EMI.
Because of our wide product portfolio, Parker Chomerics has the ability to solve many issues relating to EMI, regardless of what the underlying issue is. We have a full suite of EMI shielding products including gaskets, paints, engineered laminates, air ventilation panels, and conductive plastic pellets. This broad product range enable us to help customers do shielding at any level with the flexibility to meet their specific engineering requirements.
Learn more about high-performing EMI shielding solutions.
If you need assistance identifying the most suitable EMI shielding solution for your application, speak with one of our expert engineers. Our team is ready to help.
In this webinar on EMC Considerations for Product Designers and Engineers, you will:
With more than 60 years of experience, we have the technical know-how to meet the rapidly increasing needs of engineers.