EMI Shielding, Environmental Shielding and Thermal Management for Marine Drones - Chomerics Division | Parker US
unmanned underwater vehicles (UUVs)

Marine drones, also known as unmanned underwater vehicles (UUVs) or autonomous surface vehicles (ASVs), are becoming an increasingly critical and more common part of modern naval and maritime equipment. These vehicles have many uses, including:

  • Defense (e.g. surveillance)
  • Research (e.g. monitoring reefs or collecting samples)
  • Maintenance for oil rigs or maritime infrastructure
  • Monitoring (e.g. measuring water quality through buoy solutions)

Drones have gained popularity because of their versatility, relatively low cost compared to other monitoring/measurement equipment, and reduction of risk to operators. These drones can operate either on the water’s surface or underneath it, and some are designed to move while others are more stationary. For added flexibility, some devices can be tethered, and in other cases they utilize WiFi communication. 

Common Marine Drone Challenges

The independent nature and mission-critical operations of these applications means that great care must be taken to ensure they are durable and reliable. They face several challenges that should be considered during the design phase.

First, effective electromagnetic interference (EMI) shielding is essential. This keeps drones working effectively and doing the job they were intended to do with no disruptions or lapses in operation. Without proper EMI shielding there could be a loss of signal transmission, which could pose problems for the devices that rely on the marine drones. There are often different requirements for different types of marine drone devices.  For example, MIL-STD-461 (REQUIREMENTS FOR THE CONTROL OF ELECTROMAGNETIC INTERFERENCE CHARACTERISTICS OF SUBSYSTEMS AND EQUIPMENT) presents different emissions and susceptibility standards for Navy aircraft, submarines, and surface ships.

Environmental sealing is also critical as these devices will spend most if not all of their working times out in the ocean or other large body of water. Whether they are floating on the surface or operating deep below the surface, they will be constantly subjected to conditions including mist and salt water. In some cases, you can incorporate a dual solution in one for both EMI shielding and environmental sealing, which provides design flexibility and can reduce procurement challenges.

Finally, UUVs may need thermal management to ensure effective cooling of the navigation, monitoring, and/or data processing electronics on board. Because they’re in the water you may be able to use water temperatures to cool them to some extent, but it is also important to be able to pull heat away from the heat-generating electronics to the device housing or heat sink. 

Reliable Solutions for Marine Drones

Parker Chomerics has developed several products that are suitable for use on marine drones.

CHO-SEAL conductive elastomer gaskets, specifically materials such as CHO-SEAL 6502 and CHO-SEAL 6503, are excellent options for both EMI and environmental shielding. These gaskets, which consist of nickel-plated aluminum filler in silicone or fluorosilicone binders, respectively, suit shielding requirements of >100 dB and offer the highest performance in harsh environments.

Marine drone

For thermal management, high-performing THERM-A-GAP gap filler pads are an excellent choice to fill gaps between heat-generating and heat-dissipating surfaces. This family of compressible, thermally conductive elastomers comes in a range of thicknesses and can be provided on various carrier substrates such as aluminum foil with a pressure sensitive adhesive (PSA), a woven fiberglass sheet, a PEN film, or a Kapton liner. They offer great design flexibility as they are available as full sheets or can be cut to precise sizes and shapes to meet application-specific needs.

Focused on Our Customers’ Success

At Parker Chomerics, our customers’ success is our top priority. From our supply chain to our team of seasoned engineers, we put our customers first and ensure their needs are met.

CHO-SEAL and THERM-A-GAP products are both manufactured in the United States and bolstered by a global supply network. This allows us to meet our customers’ timelines and requirements with high-quality, reliable products without concerns for supply chain disruptions to delivery.

To further help our customers, Parker Chomerics engineers are on hand to provide design and engineering support. From selecting the right products to providing personalized design support and troubleshooting, we put our deep EMI shielding and thermal management knowledge to work for you.

Contact us today to learn about how our solutions can help keep your marine drones afloat.

Blog Post contributed by Ben Nudelman, Global Market Manager, Chomerics Division.

Get a Quote Now

Tell us a little bit about your problem and we'll do our best to come up with a cost effective, timely quote to help you get started.

EMI Shielding and Thermal Interface Solutions for Commercial and Defense Drone Technology

Advancements in drone technology come with the need to meet strict demands of lightweighting, electronics thermal management, and electromagnetic interference (EMI) shielding for uncompromising signal integrity. In this webinar our experts will provide a glimpse into the latest product advancements in Thermal Interface Materials and EMI Shielding solutions for commercial and defense drone technology. 

Parker Image

Elevating Aerial Technology: Parker Chomerics Solutions for UAVs and Drones in Commercial and Military Applications

EMI Shielding and Thermal Interface Materials

As aerial technology continues to soar to new heights, the demand for reliable solutions that ensure optimal performance and durability is paramount. Our range of cutting-edge products, meticulously engineered by industry experts, is designed to meet the rigorous demands of modern drone technology. From EMI shielding solutions to advanced thermal management materials, explore how Parker Chomerics is leading the way in enhancing the efficiency and effectiveness of UAVs in diverse operational environments.

Parker Image