THERM-A-GAP PAD - Chomerics Division | Parker US
THERM-A-GAP Gap Filler Pads

Thermal Interface Materials

Thermal gap pads are a type of thermal interface material (TIM) specifically designed to fill gaps between heat-generating electronics components and heat-dissipating surfaces. Pads are manufactured in sheets or continuous rolls at various thicknesses and are often cut to an application-specific size or shape. They are also available in a range of thermal conductivity values with higher conductivity associated with greater heat dissipation.

THERM-A-GAP PAD

Thermal Interface Material

THERM-A-GAP gap filler pads are a family of low compression force, thermally conductive, silicone pads for applications where heat much be conducted away from electronics components such as batteries, CPUs, GPUs, and microprocessors.

8.0 W/m-K High Performance, Low Oil Bleed, Low Relaxation Force Thermal Gap Filler Pad

Key features and benefits include:

  • Standard sheet stock or precut offerings   
    • Available in sheets for easy secondary manufacturing
    • Can be provide in precision cut shapes and sizes
  • High reliability
    • Shows no performance degradation after long-term aging, thermal cycling, and vibration testing
  • Ease of assembly
    • Simple "pick and place" application process
  • Multiple carrier options
    • Fiberglass carrier for ease of handling 
    • Aluminum foil carrier with pressure sensitive adhesive (PSA)
    • PEN film carrier for shear resistance
    • Kapton carrier for shear resistance and improved thermal performance
  • Low compression force
    • Applies minimal stress, making it effective for fragile electronics
  • High surface tack
  • Designed for a wide range of gaps
blue thermal interface material gap pad

Need Help Finding the Right Gap Filler? Talk to an Expert Engineer Now.

If you need assistance identifying the most suitable gap filler for your application,  speak with one of our expert engineers. Our team is ready to help.

Performance Characteristics

Low Compressions Force

Gap filler pads require slight deflection in order to make effective thermal contact between heat-generating and heat-dissipating surfaces, usually a minimum of about 5% of the nominal pad thickness. They are also a low compression force material, meaning that they require very low forces to reach ideal deflection levels and do not impart force on underlying, fragile components.

 

Gap Pad Application

Gap pads are ideal solutions for simple assembly applications. They can be provided on kiss-cut sheets or packaged based on assembly requirements. Using a "pick and place" process, gap pads can be applied manually or using an automated robot.  

Parker Image

Thermal Conductivity

Thermal conductivity of a material, typically measured in Watt per meter Kelvin (W/m-K) is a bulk material property that represents its ability to transfer heat. A higher thermal conductivity is associated with greater heat dissipation. 

 

The thermal conductivity of gap filler pads ranges from 1 to 8 W/m-K depending on the material formulation and is continuing to increase with new material developments.

70 Thermally Conductive Gap Filler Pad

Long-Term Reliability

Thermal gap pads have been around for decades and were developed for low power electronics that needed basic cooling as well as high performance, critical applications. Rigorous accelerated aging tests are performed on all materials, especially newly launched products, to help ensure long-term reliability. 

 

Parker Chomerics conducts standard, long-term reliability testing that includes compression vs deflection testing and thermal impedance measurements before and after high heat or humidity exposure.  Testing for outgassing is also conducted to ensure that silicone and non-silicone gap pads are able to meet the low outgassing requirements put in place by NASA (ASTM E595 testing). 

 

Vibration testing is also performed based on teh GMW3172 automotive test standard. Industry specific testing is available upon request to verify the effective performance of thermal gap pads in customer-specific applications.

Parker Image

Design Flexibility and Ease of Use

Thermal gap pads are preferred thermal interface material option for many product designers and engineers because of the associated design flexibility and ease of use. For prototyping, gap pads can be purchased in standard or custom thicknesses in bulk sheets or rolls. They can then easily be cut to shape. Once designed into product volumes, they can be provided as custom kiss-cut parts or kitted for ease of assembly.

Should I Use a Gap Pad or Gel?

Deciding between the thermal interface material types of gap filler pads, also called thermal gap fillers, and dispensable compounds such as thermal putties and thermal gels can be challenging. Our experts break it down so you can understand which type of thermal interface material is best for your application.

Deciding between the thermal interface material types of gap filler pads, also called thermal gap fillers, and dispensable compounds such as thermal putties and thermal gels can be challenging.Our experts break it down so you can understand which type of thermal interface material is best for your application. You won't be confused as to which thermal interface material to select after watching this!Follow Parker Chomerics: Twitter: https://twitter.com/parkerchomericsLinkedIn: https://www.linkedin.com/company/parker-chomericsSubscribe: http://solutions.parker.com/chomerics-newsletter-sign-up

Need a THERM-A-GAP GEL Instead of a PAD?

If you need assistance identifying the most suitable gap filler for your application,  speak with one of our expert engineers. Our team is ready to help.

Thermal Interface Materials

We offer an extensive range of thermal interface materials, including thermally conductive adhesive tapes, thermally conductive greases, thermally conductive heat spreaders, and thermally conductive phase change materials. We invite you to explore our selection and determine which materials are best suited for your specific application. Our products are designed with reliability and quality in mind, and our commitment to customer satisfaction is paramount.

Webinar: Selecting a Thermal Gel or Thermal Gap Pad

Discover how to select a thermal gel or thermal pad with this on demand webinar. This on-demand webinar is all about thermally conductive dispensable gels and thermal gap filler pads, focusing on:

  • How to determine which thermal interface material is right for you
  • The benefits of each - a dispensable gel or gap pad and what you need to know about them
  • Determining your requirements and selecting a material that best suits your application

Our products are used in a wide range of industries.


 

Parker Chomerics Industries

Empowering Your Business on a Global Scale

Parker Chomerics’ manufacturing operations span the globe, allowing us to serve you locally no matter where you are. We understand your unique needs and provide personalized solutions that cater to your specific requirements. 

Shop link image

Can't find what you're looking for? Talk to one of our experts.