"Cell-to-pack" (CTP) is a battery design where individual battery cells are directly integrated into a larger battery pack without additional modules or components. In this design, the individual cells are connected in series and/or parallel to create a larger battery that can provide the desired voltage and capacity. This approach is often used in electric vehicles, where the battery pack is a critical component that must be optimized for weight, volume, and energy density.
Advantages of CTP:
Disadvantages of CTP:
"Cell-to-chassis" (CTC) is where individual battery cells are integrated into a modular system, which is then connected to the vehicle chassis. The modular system typically includes additional components such as cooling systems, control electronics and safety features. In this design, the battery cells are connected to the modular system, which is then mounted onto the chassis. This approach is often used in hybrid vehicles, where the battery system is not as critical to the vehicle's performance and can be optimized for cost and reliability.
Advantages of CTC:
Disadvantages of CTC:
Choosing the right battery architecture—Cell-to-Pack (CTP) or Cell-to-Chassis (CTC), depends on the specific requirements and priorities of the EV design. Each architecture offers unique advantages and challenges, influencing factors such as energy density, manufacturing complexity, thermal management and maintenance.
Thermal management materials play a critical role in ensuring the safe and efficient operation of battery packs in electric vehicles in both cell-to-pack and cell-to-chassis designs.
In a CTP design, thermal management materials can be used to improve the heat dissipation properties of the battery pack. This can include the use of Cooltherm materials such as gap fillers and adhesives to help conduct heat away from the cells and distribute it evenly across the pack.
In a CTC design, thermal management materials can be used to manage heat and bond battery cells to the chassis and other components. This can include the use of thermal management materials to dissipate heat from the cells, regulate the temperature of the cells and prevent overheating.
Understanding the differences between CTP and CTC is crucial for manufacturers and consumers alike, as the choice of battery architecture can significantly impact the performance, safety and overall efficiency of electric vehicles. As the EV industry continues to innovate, these architectures will play a vital role in shaping the future of sustainable transportation.
Call Us at 877-275-5673
For more detailed information on EV battery technologies and to explore our range of solutions, contact us today. Together, we can drive the future of electric mobility.