Gas Dehydration - Glycol | Parker

Natural gas produced from a reservoir contains water that can cause upsets, fouling, corrosion in downstream equipment, generate hydrates formation, and can also condensate and freeze during the liquefaction process.

It is therefore mandatory to go through a dehydration step just after the acid gas removal. A glycol unit (TEG, MEG, TREG) will ensure that the water vapor entrained in the gas is absorbed in the solvent. 

 

PARKER HANNIFIN PROVIDE

  • Solids separation combined gas coalescing solution on the wet gas to absorber column
  • Liquid filters and hydrocarbon adsorbers on the rich glycol loop out and in the reboiler
  • Gas coalescers on dry gas

The wet natural gas stream enters the bottom of a contact tower (absorber) while a lean, water-free glycol is introduced at the upper section of the contactor. The glycol absorbs the water from the natural gas and the rich, water-loaded glycol is carried out the bottom of the absorber, while the dry natural gas leaves the top of the absorber and goes to further gas processing (to a gas plant or pipeline).

The rich glycol leaving the contact tower is being regenerated going through :

  • A flash separator removing coarse impurities, liquid hydrocarbon, high content hydrocarbon gas out of the glycol and decreasing the pressure
  • A stripping / distillation column called reboiler working between 100-200°C, where water is distillated out to recover glycol high purity
  • A flash tank
  • A series of particulate filter, protecting an activated carbon adsorber for liquid hydrocarbons degradation products removal

The hot, lean glycol is cooled down in two steps, repressurized and fed back to the top of the contact tower.

Upgrade your Midstream Oil & Gas Process to the Next Level

 

Dive deeper into our filtration solutions for midstream applications including:

  • Acid gas removal
  • Mercury removal
  • NGL recovery
  • NGL fractionation

Need Help?

Can't Find What You're Looking For? Get in Touch With One of Experts