RICHMOND, Cali., March 31, 2023 — The Veriflo Division of Parker Hannifin Corporation, the global leader in motion and control technology, announces the expansion of FR Series pressure regulators for semiconductor gas delivery with the addition of the FR1300 and FR1403SA models. These regulators complete the product line that already includes the FR1000, FR1200, and FR1400, providing more options to our customers and meeting the evolving needs of the semiconductor industry. With nearly 60 years of experience in gas delivery systems, we are confident that the FR Series will continue to deliver the precision and reliability that our customers expect.
“The full FR Series product line gives customers the flexibility to choose the regulator that best suits their specific needs,” said Samson Lin, Veriflo Division Product Manager. “With the addition of the FR1300 and FR1403SA models, the FR Series pressure regulators now offer a complete product line to meet the diverse needs of semiconductor fabrication gas delivery processes and gas delivery systems.
The FR1000 continues to be the go-to regulator for valve manifold boxes, gas cabinets, and various other point-of-use applications. The FR1200 and FR1300 models provide enhanced capabilities for point-of-use bulk gas and specialty gas applications, making it easier for customers to operate different process applications with more options. Meanwhile, the FR1400 is the ideal choice for cylinder or point-of-use bulk gas applications and specialty gas applications. Finally, the FR1403SA is perfect for customers who require negative delivery pressures with low-pressure gas sources.
The Parker FR Series, in combination with the current premium Parker Veriflo line of regulators, will enable Parker to close key product line gaps to serve a wider range of applications in semiconductor fabrication. The FR Series is optimized for Ultra-High Purity (UHP) semiconductor gas delivery and provides multiple end connection size and types for easy installation. In addition, the FR Series is available in fully configured gas sticks, which streamlines the ordering process and reduces lead times for customers. With this expanded product line, Parker is well-positioned to meet the needs of its customers in the semiconductor industry.
About Veriflo Division
Veriflo is Parker Hannifin’s global leader in the semiconductor industry and a leading manufacturer of precision diaphragm and bulk gas valves, regulators, and flow control components for the control and application of liquids and gases.
About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
###