The Parker Difference - Tube Fittings Division | Parker US
Parker Image

ToughShield® Plus achieves the highest corrosion-resistance performance levels, even for crimped products, without impacting other parameters such as assembly procedures, pressure, and performance, along with compatibility with existing products.

Rethinking Zinc-Nickel Plating

Parker's goal has been to take zinc-nickel plating, which already offers good performance in most applications, to the next level. Historically, a drawback of zinc-nickel plating for fluid power connectors has been its impact on assembly. Zinc-nickel and zinc have different physical properties. Zn-Ni plating is rougher due to a different crystal structure and therefore has a higher coefficient of friction. This, in turn, means there is a requirement for higher assembly torque or turns to provide appropriate connection loading for a safe and leak free connection. Zn-Ni also hasn't performed well on parts with post plating deformation, like crimped nuts. These surfaces can corrode more rapidly due to the plating being compromised by metal deformation.

 

Parker's aim was to create a plating that achieves the highest corrosion-resistance performance levels, even for crimped products, without impacting other parameters such as assembly procedures, pressure, and performance, along with compatibility with existing products. This was accomplished by studying and better understanding the relationship between metal structures, properties, and processing – all validated under controlled conditions.

ToughShield Plus - Rethinking Zinc-Nickel Plating

The Parker Difference

Parker's engineering and metallurgy experts, working closely with our customers, are continuously dedicated to fundamentally understanding the cause of corrosion and how it progresses. Their commitment ensures that our customers' systems perform better and last longer, saving them costs. As a result, the new ToughShield™ Plus plating offers a significant improvement to corrosion resistance versus other available plating technologies.

Parker Image

Premium Plating Performance Validation

Parker engineers and metal scientists used state-of-the art tools and analysis methods to study corrosion and how to minimize it. This led to the development of our patent-pending advanced plating which provides superior corrosion and assembly performance, even on products subjected to after plating deformation such as swivel nuts and other fluid power components.

 

The superior corrosion resistance of Parker's latest plating technology is validated through ASTM B117 / ISO 9227 neutral Salt Spray Testing (SST), as well as two Cyclical Corrosion Tests (CCT) - ISO 16701 and SAE J2334. CCT is widely considered to provide a closer correlation to field corrosion conditions. ToughShield Plus is the first standard plating system in the fluid power industry proven to offer this exceptional level of resistance to red rust.

Premium Plating Performance Validation
Download the Whitepaper

Scientists and engineers at Parker worldwide have pooled their metallurgical know-how to deliver next-generation plating technologies. This provides a leap forward in long-term anti-corrosion performance while maintaining compatibility with existing products and without impacting assembly procedures and performance benchmarks.

Download the whitepaper to learn more about the extensive research and development of ToughShield Plus.

Advantages of ToughShield Plus

The advantages of Toughshield Plus and the true cost of corrosion goes beyond just replacing a tube fitting or adapter. Since corrosion can affect every aspect of your system, the advantages of using ToughShield Plus are far reaching:

Extended Fitting & Adapter Life

Extended Fitting & Adapter Life

ToughShield Plus provides significantly longer corrosion resistance which means extended service life for your equipment's systems, higher productivity for your personnel, and ultimately more revenue for your operation.

Easier & Less Frequent Maintenance

Easier & Less Frequent Maintenance

Rusted tube fittings and adapters, as well as adjacent components, are more difficult to disassemble and replace when "rusted" together and wrenching surfaces are compromised. ToughShield Plus prevents rust and its migration longer than the industry standard, making routine maintenance easier.

Increased Resistance to Corrosion Migration

Increased Resistance to Corrosion Migration

Once corrosion consumes the fitting/adapter surface, it can accelerate by migrating to other components such as a cylinder boss or valve. This leads to the need for earlier, more frequent, and more costly repairs. ToughShield Plus fights corrosion longer, providing critical defense for your system.

Increased Equipment Uptime

Increased Equipment Uptime

When equipment and the personnel who operate them aren't working due to maintenance from corrosion, this downtime can lead to loss of revenue and reputation, as well as the total cost of ownership (TCO) of the equipment. ToughShield Plus plating fights corrosion longer, ensuring more uptime.

Prevents Aesthetic Quality Concerns

Prevents Aesthetic Quality Concerns

Rusted components on equipment affect the overall aesthetics leading to a lack of confidence in the equipment and a hit to the manufacturer's reputation. ToughShield Plus plating fights corrosion, and the migration of corrosion, longer protecting the integrity of the equipment and operation.

Saves Warranty Costs

Saves Warranty Costs

For equipment manufacturers, tube fittings and adapters that corrode quickly can lead to warranty claims and loss of reputation. ToughShield Plus helps prevent corrosion longer in systems, preventing costly hits to the bottom line.

Consistent Process & Continued Performance

Throughout the ToughShield Plus plating development, there was a strong focus on process stability and control. The principles of statistical process control were implemented on critical production variables with strict monitoring procedures and control limits established to assure ToughShield Plus performs uniformly throughout the broad Parker product range and numerous global plating operations. As a result, the high process capability of the ToughShield Plus plating system has been demonstrated for a mass production environment. The robust process has little variation from day-to-day operation and from part-to-part on the same day.

 

ToughShield Plus was created for a seamless transition into customer systems, offering full compatibility with the zinc and zinc-nickel plating on current Parker fittings.

This means customers can expect no changes to Parker’s current: 

  • Assembly procedures
  • Pressure ratings and performance
  • Industry specifications and approvals
  • Paintability
  • Environmental compliance including REACH, RoHS and ELV

  

Where to Buy

Interested in getting ToughShield Plus for your hydraulic tube fittings or adapters? Parker’s worldwide distribution network makes it convenient to get the parts you need, either over the phone or at one of our Parker Stores. Locate the distributor nearest to you.

Proving Performance

Testing, optimization and analysis of ToughShield Plus is critical to ensuring performance criteria was met. Corrosion is not a property of the material or an individual part – it is always the result of a combination of ambient conditions – each of which can impact the performance of metal parts and components at their final point of use.

During the development of ToughShield Plus, Parker completed ASTM B117 neutral salt spray tests, as well as CCT tests, like ISO 16701, which are industry accepted tests to prove performance in highly corrosive environments.

Parker Image

State-of-the-Art Metallurgical Labs

Investing in state-of-the-art equipment and technologies, while working closely with our customers, Parker engineers and scientists utilize our metallurgical laboratories to simulate real-world applications and study and understand plating on a microscopic level.

 

ToughShield Plus was created using methods like scanning electron microscopes and x-ray machines, as well as electrochemical analysis methods such as impedance spectroscopy to reveal and study highly detailed surface characteristics. External and internal industry salt spray and CCT testing were also conducted and studied to validate the process and performance.

 State-of-the-Art Metallurgical Labs

Have a Question?

Want to know more about ToughShield Plus and how it can benefit your application? Need more information about our tube fittings and adapters? Our customer service team is ready to assist you with any inquiries or questions you may have. You can also check out our Support section for additional information.