Cost of Corrosion - Tube Fittings Division | Parker US
Parker Image

Corrosion means more than simply replacing the failed components - it also results in more downtime and high costs from additional maintenance and warranties.

Facts About the Cost of Corrosion

Tube fittings and adapters are used in a wide variety of applications around the world. They are often exposed to mechanical and physical stress, which can accelerate corrosion. Especially smaller, relatively inexpensive components can be replaced quickly. Corrosion control does not seem to be a particularly important task, however, the cost of corrosion is much higher than most people realize.

What would you estimate are the costs caused by corrosion worldwide?

According to one of the world's leading research institutions dealing with corrosion and its consequences, NACE also published a report on the costs caused by corrosion worldwide. According to the report, it is approximately $2.5 trillion or 3.4% of global GDP. These costs do not yet include environmental damage or safety hazards to people. With more effective measures to counteract corrosion, the monetary costs incurred could be reduced by 15-35% (US$375-$875 billion), according to NACE - not to mention the increased safety for people and the environmental consequences, both of which are not included in these numbers.

The cost of corrosion has an impact across industries worldwide

(Source: http://impact.nace.org/documents/Nace-International-Report.pdf)

True Cost of Corrosion

Corrosion is not just an unsightly inconvenience, it's also a costly drain on operating and maintenance budgets. The full cost extends beyond the expense of replacement fittings or even more costly adjacent components – but also to equipment downtime. When valuable equipment is underutilized with skilled operators idle, this magnifies these losses. Downtime can lead to losses of revenue, reputation and customers.

Shorter Fitting & Adapter Life

Shorter Fitting & Adapter Life

Corrosion can happen at any time in nearly every environment, taking hold quickly and consuming the fitting. This leads to shorter steel tube fitting and adapter life, as well as migration to corrosion and more difficult maintenance.

Frequent & Difficult Maintenance

Frequent & Difficult Maintenance

Corrosion can affect the integrity and performance of fittings and adjacent components, creating a need for more frequent maintenance. It can also make service and repairs more difficult as mating components tend to be "rusted" together and wrenching surfaces may be compromised..

Corrosion Migration to Adjacent Components

Corrosion Migration to Adjacent Components

Once corrosion starts, it is difficult to stop, spreading quickly from tube fittings, for example, to other adjacent critical and more expensive components. Protective measures such as using tube fittings and adapters with ToughShield® Plus plating safeguards against corrosion longer.

Costly Downtime

Costly Downtime

When corrosion infects a system, the full costs extend beyond the expense of replacement fittings to costly adjacent components and also equipment downtime. When valuable equipment and skilled operators are idle, this can lead to losses of revenue, reputation and customers.

Aesthetic Quality Concerns

Aesthetic Quality Concerns

When corrosion infects a system, it can affect the overall aesthetics, which leads to a lack of confidence in the equipment and a costly hit to the brand reputation.

Potential Warranty Claims

Potential Warranty Claims

When corrosion takes hold and quickly infects an entire system, it can mean costly warranty claims that could have been avoided.

Tell us about your application, request technical or engineering support, or send us your question about ToughShield® Plus. Our customer specialists are ready to help.

How Corrosion on Steel Forms & Spreads

How Corrosion on Steel Forms & Spreads

Corrosion occurs primarily where metal is exposed to environmental influences and/or harsh chemicals or media in the application. Salts in the air, humidity, minerals (e.g. mud or soil), and rain, including an application's harsh chemicals or media, can all accelerate corrosion.

In the scientific sense, corrosion is an electromechanical reaction in which atoms begin to move. As illustrated in a corrosion cell above, electrons and ions flow through a metallic path where anodic reactions are occurring to sites where they allow cathodic reactions to occur. The metal surface becomes rougher and thinner. Once this reaction starts, it is difficult to stop. Corrosion spreads quickly, for example, from tube fittings and adapters to other critical and more expensive components.

This is why it is important to consider corrosion when sourcing and installing / replacing tube fittings and adapters in your systems.

Disadvantages & Consequences of Corrosive Parts

Disadvantages & Consequences of Corrosive Parts

Corrosion is associated with several disadvantages that affect not only the individual, corrosive component, but possibly the entire equipment. For example, if hydraulic lines leak due to corrosive fittings, the entire machine usually stops. Depending on where the equipment is located, repair involves a lot of downtime during which the equipment is not making money while incurring costs.

If corrosion spreads from less expensive components to more expensive ones, the damage and expense is even greater than just the replacement of the parts. For equipment manufacturers, early component failure and the resulting reduced uptime can also be associated with high warranty costs. Additionally, the OEM's brand image can suffer as a result of early corrosion and equipment failures.

As you can see, corrosion can have significant operational and economic consequences.

Where to Buy

Interested in getting ToughShield Plus for your hydraulic tube fittings or adapters? Parker’s worldwide distribution network makes it convenient to get the parts you need, either over the phone or at one of our Parker Stores. Locate the distributor nearest to you.

Where to Buy