Parker Hannifin’s Hydraulic Pump and Motor’s engineers walked OEM Off-Highway readers through the conversion process from an Internal Combustion Engine (ICE) to electric by focusing on key considerations and tools to aid in this migration. Through Parker HPM's presenters, the webinar focused on: What key factors OEM's need to consider when changing from ICE to electric, How to choose the correct system components from both a size and selection perspective, and what to look for in an engineering partner.
Learn how Parker and Summit Attachments reached new heights with Parker's V16 variable motor technology. Summit Attachments and Machinery is a company that utilizes existing platform frames and reworks the equipment adding their custom attachments for specific, rigorous applications within forestry.
To continue to improve upon their Winch Assist Systems, which offers up to a 55,000-pound pull effort and is crucial to steep slope harvesting, Summit collaborated with Parker’s Hydraulic Pump and Motor Division and a Parker distributor, Motion & Flow Control Products, Inc.
Learn how ePumps are evolving with hybrid and electrification applications through a video Q and A session with Parker HPM's Engineering and Business Development Manager, Rob Lorance and the publication Machine Design.
A large automotive manufacturer was in search of a turnkey supplier to design and construct a large, central hydraulic system capable of providing stable hydraulic oil pressure at variable volumes. Learn how Parker and Exotic Automation and Supply collaborated to create this new hydraulic system that increased overall efficiency, while reducing energy waste.
Learn how Parker and Allied Systems, a Portland, Oregon-based fabricator of material handling equipment for the wood products industry, worked together to redesign the hydraulic system of their New Generation series Wagner L490 Log Stacker for greater efficiency. Before the redesign, the L490 took 18 seconds to lift a 45-ton payload from the ground to the top of its lift height of just over 19 feet. With a revised hydraulic system that has twice the hoist speed of the earlier design, Allied Systems was able to significantly reduce cycle times over the previous model L490 by two to one. The major components of the new L490 design include a wide variety of Parker Components, including P3 Pumps, M5 Fan Motors, K220LS and M402LS Valves, IQAN Controls, and Display Electronics.
Learn how Parker and K&B Lumber worked together to innovate sawmill technology in order to increase the production of high-quality lumber for the furniture industry. For the saw’s power source, a Parker Gold Cup P14S Pump was selected, driving a Gold Cup M20R Motor stacked with a Parker F12 Series Bent Axis Motor on the back. This powerful combination allowed for additional system displacement. Overall, K&B Lumber has benefited by a smaller, safer sawmill. The new sawmill has also resulted in more efficient energy usage, while producing more output.
Learn how Parker and Eco Green Equipment collaborated on the hydraulic system for a mining tire recycling equipment. Through the Parker F12 hydraulic motors, the equipment has the capability, efficiency, and longevity to cut through the mining tires’ tough rubber layers on a consistent basis.
Learn how Parker collaborated on the hydraulic system for Eco Green's Krumbuster, revolutionizing crumb rubber production with key hydraulic components including Parker P24 and P6 Gold Cups and T6 Vane Pumps. These Parker pumps were chosen to complement the hydraulic motor due to their reliability, responsiveness, and ability to handle a high shock load.
Learn how a next generation mobile pump, P1M, increases construction equipment performance. The new P1M Series was developed specifically for the OEM mobile application market and is more compact with its patented inlet design, which provides higher power density, best-in-class speed ratings and longer life expectancy.
Learn how Parker and Rayco collaborated on the design of a new stump cutter by recommending an alternative to a competitive closed-circuit pump and exceed performance targets. Results include an increased system efficiency by 10% over competitor test units, a 10% increase in cutter wheel torque output, and a 20% decrease in heat generation.
Learn how Parker’s Global Mobile Systems (GMS) redesigned a sugarcane harvester's hydraulic system to improve efficiency and reduce system complexity. Results of the redesign include: increased power management, fuel savings, increased machine productivity, and lower system costs.
Gold Cup piston pumps and motors set the bar for severe duty hydrostats, with design features that extend life, increase productivity, and reduce energy losses. Its robust barrel bearing design, hi-shock capabilities, precise controls, hi-flow ring checks, and auto regulating servo are just a few of the standard features that provide performance in this series up to 3600 rpm and 6000 psi (420 bar). Gold Cup's high power-to-weight ratio and flexibility in control options deliver significant value-added benefits.
Fracturing trucks are the main equipment type utilized for fracturing construction in oil and gas fields. These trucks’ main function is to inject high flow and pressure fracturing fluid into the oil and gas field, which in turn, creates fractures in the rock formations. Learn how a fracturing truck manufacturer selected our Gold Cup Series for its reliability, stability, and competitive performance.
A stainless-steel producer was experiencing hydraulic pump failure on a variety of pump manufacturers’ products, including a Parker pump. The manufacturers’ hydraulic pumps would have an approximate one-month life and then fail. Learn how Parker identified and solved their problem resulting in a 1700% improvement in pump life.
The selection of a motor for a hydraulic application can be complicated. The ideal in hydraulic system design is to match overall efficiencies to the application performance expectation. This Whitepaper will explain how to select between various hydraulic motors, namely: Gear, Vane, Piston and Radial Piston.
Hydraulics & Pneumatics, October 2010 - The ultimate goal for a shredding system is to reduce the source material-appliances, tires, concrete, etc, - to smaller particles for recycling. To transmit the kw-speed, high-torque power needed for these heavy-duty shredders, a gearbox could be used to reduce speed from an electric motor while multiplying torque. However, hydraulics technology is a more practical solution both for systems driven through gearboxes and those that utilize low-speed, high torque motors in direct-drive systems.
Hydraulics & Pneumatics, July 2010 - The pumps used in Columbia's walking system drive are Parker Hannifin T6CC vane pumps, which provide a single inlet and two outlets. Designed to be self-wear compensating, these pumps tolerate contaminates and maintain high efficiency over their service life. High efficiency means an overall longer life for the hydraulic system. High lifetime efficiency ensures safe and reliable output from the pumps throughout their service.
Due to BMH customers’ demand needs for almost 24/7 equipment uptime, BMH needed to find a reliable hydraulic component supplier to operate their TYRANNOSAURUS Shredders and Crushers with as little downtime as possible. Parker’s Gold Cup Hydrostatic Pump and Motors were a key component selection since they supply the hydraulic power to operate the TYRANNOSAURUS Shredders and Crushers. Learn why Gold Cup was selected and what results it delivered.
Parker frameless motors have been specified into a series of lunar rovers, which will be making their way to the moon over the next several years. The motors are being used to rotate the lunar tires that propel the vehicles across the moon’s surface.
Diesel, January 2023 - Parker seeks to ease OEMs’ path to electrification, starting with hydraulic systems. OEMs continue to seek a broader range of solutions to meet customer and industry demands for ever greater efficiency, with some going all in on power system advancements like electrification. Yet, when it comes to motion, Chris Griffin, group business development manager, electrification, at Parker Hannifin’s Motion Systems Group, believes it doesn’t have to be an all-or-nothing approach.
While developing its next generation of electric buses, a leading bus manufacturer, reevaluated every aspect of the existing design elements to uncover ways to improve power density, reduce packaging size and weight, lower noise emissions and increase system efficiency as well as improve passenger and driver elements. Parker’s design included the integration of all electric components into the gear box: the electric motor, inverter, transmission, integrated cooling system and service brake. This high degree of integration reduced the number of interfaces to the vehicle and reduced the number of components and therefore, reducing the footprint and weight.
A job that involved multiple divisions of Parker Hannifin Corporation illustrates the staggering complexity of design and development projects of this type. Parker was approached by a well-known maker of commercial and executive jets for assistance in developing a new flap control system, including the flap power drive unit (PDU), for its new business jet.
Learn how Parker and an automation customer designing an autonomous vehicle that would collect grocery items from a warehouse and then deliver them to a central drop-off location for curbside grocery pick-up, designed a motor to drive the wheels of this vehicle. The customer benefited through increased efficiency and reduced operating costs.
Learn how Brammo emerged from the exhilarating motorcyle racing event, Isle of Man TT, to engineer the world's fastest production electric motorcycle. Brammo partnered with Parker for a venture into uncharted territories of motor development. Through rigorous brainstorming and collaborative problem-solving, teams worked together to configure Parker’s electric Global Vehicle Motor (GVM) into a marvel of engineering tailored for the Empulse R electric racing bike.
Novum Tech and Parker Hannifin formed a close partnership for the future of agricultural electrification. The challenge they faced was to electrify a combustion tractor at a controlled cost, while maintaining low voltage, which limits power. The solution was a dual-motor solution that improved performance, operated quieter, and eliminated CO2 emissions than its diesel counterpart.
See how Parker's right-angle gearbox met the requirements of a customer's demanding application in the data security market. A data security customer that builds intelligent tape libraries for archieved, tiered storage workflows was seeking a compact linear actuator solution. The product solution Parker provided for their unique application was a customized RS -Series - Gen II Stealth High Precision Right Angle Helical Planetary Gearhead.
Please check out HPM's additional resources, including:
For local support and service, please contact your local, authorized Parker Distributor.
Parker's worldwide distribution network makes it convenient to get the parts you need, either over the phone or at one of our Parker stores.
To find your Parker Distributor, please use the Where to Buy link above.