Automation technology generally deals with workflows in industrial production processes, i.e. the utilization of control and processing functions that start, monitor and end individual or interlinked work processes of machines. Efficiency and safety play a major part in this. Measurement and control units are just one of many examples of possible applications as automation is found at all human-machine interfaces. The wide-ranging potential of designing production steps is matched by the wide range of sealing systems for the respective application profiles. With an extensive portfolio of established sealing solutions extending from O-rings to rod and piston seals to application-specific solutions Parker Prädifa offers perfect prerequisites for long lifecycles.
The capabilities and reliability of rolling bearings are in large part determined by the materials used to manufacture the individual components. Rolling bearing cages are subjected to mechanical stress exerted by friction, tugging and inertia forces. In addition, there may be chemical effects due to certain lubricants or additives, organic solvents or coolants. The significance of the individual properties also depends on the operating conditions such as a humid environment, higher temperatures, impact loads or combinations of these. Seals integrated in rolling bearings may considerably affect the performance and reliability of a bearing as well. The seal materials must be resistant against oxidation (aging), wear and chemicals across a wide temperature range. With a wealth of experience in materials engineering and the respective seals and elements Parker Prädifa helps ensure that bearing deliver smooth performance.
Drive technology is an important technical discipline in mechanical engineering and adjacent fields. Its uses include actuator technology, precision engineering, medical device technology, automotive engineering, aerospace engineering, railway engineering and many other technical disciplines. Likewise, drive technology becomes an object for control and automation technology. The fields of application are as extensive as the diversity of drive systems and thus the sealing systems they use. The latter require special designs for the respective requirements to ensure perfect performance. With numerous established sealing solutions from O-rings to rod and piston seals to application-specific solutions Parker Prädifa offers perfect prerequisites for long lifecycles.
Electric motors can be found practically anywhere today. In industrial environments, electric motors are used to drive machines and forklift trucks but also for controlling industrial robots and cranes. Commuter and subway as well as many long-distance trains are powered by electric motors, too.
In addition to long maintenance intervals, service life and robustness, efficiency is a key requirement. Maximum output combined with minimal energy consumption is a focal point in development, not only with respect to energy consumption but also in terms of design size and weight. The higher a motor’s power-to-weight ratio is the smaller is its possible design. To achieve this, the subcomponents of a motor such as bearings, guides and seals should operate with low friction in order to avoid excessive losses in an electric motor’s drive energy. With many years of experience in the development of low-friction and energy-efficient sealing systems and the requisite materials Parker Prädifa offers suitable solutions for use in electric motors.
Actuators are required for applications involving the execution of linear motion. In the packaging industry, they move the arms of pick-and-place machines or sliders to eject faulty products. Actuators in the process industry serve to open and close gates/doors, slides and valves. An electromechanical actuator is a combination of an electric motor, a transmission and a threaded spindle that transforms a rotary into a linear motion. To ensure perfect performance of the individual components, the sealing concept has to satisfy the friction, tightness and resistance requirements as well. Parker Prädifa offers appropriate sealing concepts ensuring long actuator life.
Industrial transmission systems are used in practical all industrial areas and come in all conceivable sizes and forms. They have to meet extremely diverse operating requirements and operating conditions. Irrespective of the sector in which they are used, all industrial transmissions must operate as reliably and efficiently as possible and the diversity of transmission solutions in industrial applications makes maximum demands on the development and manufacturing expertise of the producers. At the same time, this diversity spawns an enormous range of operating conditions and thus influences the selection of sealing materials and geometries to be considered. In the absence of universal rules for the selection of the suitable type of seal for a particular application, Parker Prädifa offers expert assistance in selecting the seal best suiting the respective application.
Linear technology is a technical sub-discipline of drive technology. It deals with mechanical components or mechatronic systems to execute translatory movements. Characteristic for linear guides and drives are low-friction running and the ability to absorb lateral forces without deformation. Linear modules and linear tables are particularly important in factory automation, electronics and semiconductors production, the medical device and pharmaceutical industries, and in the food and packaging industries. These markets require customized solutions for gripping, lifting, turning, positioning and depositing. Every application requires an individual solution and thus an individual sealing technology solution as well. Parker Prädifa develops such solutions together with the customer to specifically suit the customer’s needs.
Machine tools require robust and long-lasting sealing and guiding elements from a proven seals and materials specialist. With a wide range of hydraulic, pneumatic and rotary seals and materials adapted to them Parker Prädifa offers the right solution ensuring the perfect interaction of the individual machine elements.
Measurement and control technology is playing an ever more important role in an increasingly automated world. Parker Prädifa offers an extensive product portfolio of sealing solutions for a wide range of applications.
Catalogs
O-Ring Handbook
O-Ring Guide