Find out why Black Eagle hose, HCR collapse resistant hose and Parker hotline hoses excel over other hoses.
Substantial new midstream infrastructure will be needed by 2025. See how Parker is meeting the challenge.
Improve service life with proven motion and fluid control hoses. CNG, LPG and Hydrogen solutions.
Featured Hose
Flexible Large Bore UHP Hose
Parker is the only oil and gas hose manufacturer featuring ColorGard™ Technology. ColorGard™ acts as an “early warning” indicator which involves an additional colored sheath extruded between the jacket and the wire reinforcement and serves as a visual indicator to alert the end user of excessive external abrasion which has potentially compromised the operational integrity of the hose assembly.
Umbilicals
Parker builds BOP umbilicals with small O.D. velocity hose, allowing for precise control and faster response times. Parker hotline hoses for BOP control act as the primary emergency hydraulic control line. If the hydraulic control line of the BOP fails, the hotline would shut down the well valve and trigger the Emergency Disconnect System. In these critical applications, nothing is more important than fast response to ensure the safety of operators.
Read our blogs to learn more about our products and technologies.
Overview of hoses by by pressure and size
Parflex custom designed oil and gas hoses have smaller O.D’s and feature fast response time for precise control on BOP applications. Other advantages include long, continuous length and extreme abrasion resistance.
Parker Hannifin Parflex Division
N.A. | Ravenna, OH USA
Parflex is a solution partner for engineered polymer-based hose and tubing. We develop products that extend the life of our customers equipment, and where possible, increase safety for operators.
Parker Hannifin Parflex Division
N.A. | Ravenna, OH USA