A material certificate, also known as a mill test report (MTR) or mill test certificate (MTC), is a crucial quality assurance document used in the metals industry. It certifies a material’s technical parameters, such as its chemical composition, mechanical or physical properties, manufacturing routes, heat treatment details, testing results, and compliance with international or local standards.
Material certification serves as the unique identifier for a particular material heat and production batch. It provides information about the material’s provenance, quality, and potential performance under real-life service conditions.
Several industry standards establish harmonized formats for material certificates, with ISO/EN 10204 being the most widely used. Among these, the 3.1 type certificate is the most common.
In Fig. 1, we see a standardized 3.1 certificate with limited information, containing only the mandatory parameters prescribed by the standard.
This includes basic chemical and mechanical properties, but it is insufficient for full traceability or determining the alloy’s quality and final properties.
Critical missing details include:
Furthermore, there is no assurance that the material is free from contaminants like mercury, or other hazardous substances, a common concern in an industry where a significant percentage of steel is recycled and re-melted.
In contrast, a certificate with a higher level of detail is usually indicative of high-quality materials and tightly controlled processes. Such certificates enable full traceability of the manufacturing cycle on any production batch, from melting to the finished component.
Fig. 2 exemplifies a good certificate that offers extensive material traceability. It includes detailed information on:
This comprehensive data compilation allows for a fully controlled quality system, ensuring the material’s reliability and safety in demanding applications.
An example of a 3.1 material certificate with limited information on material traceability.
An example of a certificate highlighting key parameters. This image shows only one page, additional details are provided on other pages.
In industries, where material quality and traceability are paramount, the level of detail in material certificates can make a significant difference. High-quality certificates provide assurance of the material’s provenance, processing history, and compliance with stringent standards, thus ensuring the integrity and performance of critical components.
At Parker, we pride ourselves on sourcing materials for our components that come with comprehensive and detailed material certificates. These high-quality certificates ensure that our materials meet the highest standards of quality and traceability, providing our clients with the confidence they need for their demanding applications. With decades of experience in material science and thousands of successful applications, Parker is your trusted partner in ensuring the highest standards of material quality and performance.
As a source of clean energy, hydrogen is making a great contribution to a more sustainable future. However, it can embrittle poor quality steel materials, leading to unexpected component failures. This article looks at how materials certificates can protect OEMs from such problems.
The Oil and Gas industry sector is driven by safety and has been for over 60 years around the globe. Whilst the industry has had issues with incidents, it has been proven that by adhering to good working practices and following recommended installation techniques and procedures, these incidents can be minimized.
Selecting materials for a given application is one of the main design steps towards a safe and cost efficient system, yet a commonly overlooked stage, mainly performed from a purely economic standpoint. The benefits of selecting the best candidate alloys and controlling corrosion are numerous and include asset safety and integrity, optimum performance with minimal maintenance and shutdown time or longer life expectancy. All those these advantages ultimately lead to considerable cost savings.