Parker’s new tyre-actuated globe valve delivers safety to cryogenic transport trailers with speed, convenience and reduced weight - Instrumentation Products Division | Regional English sites
tyre-actuated globe valve

Pneumatic tyre-actuated globe valve is the latest addition to Parker’s comprehensive Bestobell cryogenic valve range

Learn more about the Parker Bestobell globe valves at: 

https://ph.parker.com/gb/en/cryogenic-globe-valves

Barnstaple, UK, 21st June 2023 - The Instrumentation Products Division Europe of Parker Hannifin, the global leader in motion and control technologies, today announced the addition of a tyre-actuated pneumatic valve to its Bestobell cryogenic globe valve range. The valve can be operated remotely with a single switch command, providing much greater speed and convenience than a manually operated type.

 

The tyre- actuated pneumatic valve complements the Parker Bestobell range of cryogenic valves, which covers gate valves, ball valves, check valves and relief valves as well as globe types. It comes with all the same features, specifications, and certifications as the manually operated valves, and is available in the following valve sizes: DN25, DN40 and DN65. It also has various end connections, including butt weld, socket weld and flanged.

 

Globe valves are used for pressure and flow regulation as well as shut-off. The tyre-actuated globe valve is particularly beneficial to cryogenic transport trailers, as its rubber actuator weighs significantly less than stainless-steel linear actuators. The valve features a longer, stronger spring to assure a robust seal on closure – an essential safety consideration. Remote control allows emergency operation; the valve can also be integrated into an automated system, or installed in inaccessible locations. Manual override is provided to perform an emergency discharge if air pressure is lost.

 

“We developed this product because cryogenic trailer operators were seeking a lighter version of an actuated valve,” said Olga Krasilnikova, Parker Bestobell cryogenic valves product manager, Instrumentation Products Division, Europe. “Not only does it mean that operators can safely save time and effort every time they use the trailer, but also its reduced weight will contribute to better fuel economy. This is an essential consideration for both cost-saving across the vehicle fleet and improving sustainability for the company.”

 

 

About Parker’s Instrumentation Products Division, Europe

The Instrumentation Products Division, Europe provides highly engineered pressure and temperature process control instrumentation and systems. These range from compression tube fittings, cone and thread fittings, needle valves, ball valves and compact stream-switching valves to modular process and instrument valve packages. These items are all developed and manufactured to increase customers’ up-time, maintain safety, and improve production and quality control. Learn more at www.parker.com/ipd.

 

About Parker Hannifin

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century, the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.

MEDIA CONTACT

Olga Krasilnikova
Instrumentation Products Division, Europe
Phone: +44 (0)1271 313131
Email: olga.krasilnikova@parker.com

Lisa de Beer
Public Relations EMEA
Parker Hannifin
Phone: +27 (0)11 961 0700
Email: lisa.debeer@parker.com