Challenge
Supply an ambitious and growing company with EC-79 approved tube fittings as part of a pioneering dual-fuel hydrogen retrofit solution for commercial vehicles.
Solution
Parker could offer ULEMCo local stock of EC-79 Certified A-LOK tube fittings via an authorized Parker Partner who ensured availability of fittings in various sizes.
BENEFITS
ULEMCo can feel confident that the tube fittings will function as expected without leaks. Fast access to local stock ensures flexibility and no impingement on lead times. Single-source supply for both tube fittings and pressure relief valves. Access to Parker’s comprehensive engineering support
CUSTOMER COMMENT
Amanda Lyne, Managing Director and co-founder of ULEMCo Ltd
PIONEERING A DUAL-FUEL HYDROGEN SOLUTION
Liverpool, UK-based ULEMCo was born in 2014 to commercialise intellectual property and capability in hydrogen combustion engine technology. ULEMCo solutions allow commercial vehicle fleet managers to reduce their carbon emissions to ultra-low levels. The vehicles benefit from a reduced carbon footprint while still achieving the full range capability of standard diesel vehicles. “Having worked in hydrogen and fuel cells for some time, I’m passionate about delivering solutions for customers that will actually make a significant difference to carbon emissions now, not sometime in the future,” states Amanda Lyne, Managing Director and co-founder of ULEMCo. “Council vehicles such as road sweepers, refuse trucks and road gritters are ideal for our dual fuel hydrogen technology as they return to base for refuelling as part of their duty cycle.”
A CAPABLE AND WILLING PARTNER
“At the start of our journey, we needed to source EC-79 tube fittings at a time when there were limited options available,” explains Amanda Lyne, who is also Chair of the UK Hydrogen and Fuel Cell Association. Prior to Parker’s involvement with ULEMCo, the company had commenced the process of submitting its A-LOK® tube fittings to the EC-79 certification process. This development was of obvious interest to ULEMCo, putting Parker in prime position to become the preferred supplier. ULEMCo also makes use of Parker tools to ensure the correct pre-assembly of A-LOK® two ferrule fittings on the tubing. This requirement stemmed from the participation of ULEMCo in Parker’s New Product Blueprinting discovery session on alternative fuels, which indicated the benefits available from using a preassembly tool. The tools clamp into bench-mounted vices at the company’s facility, where they offer a 20% time saving in comparison with manual installation. ULEMCo has completed over 100 vehicle conversions to date. A three-cylinder system conversion, for instance, will feature up to 30 Parker A-LOK® EC-79 certified two ferrule tube fittings, plus a Parker HPRV proportional relief valve. “Everything we do here at ULEMCo is based on an established safe process,” says Amanda Lyne. “Parker HPRV series relief valves are a safety-critical component. Together with the tube fittings, Parker has become a vital part of our hydrogen safety story.
TECHNOLOGY THAT MAKES A DIFFERENCE
ULEMCo’s dual-fuel solutions displace 30-70% of the energy that would normally come from diesel, with hydrogen. Almost any type of HGV (heavy goods vehicle) is suitable for conversion and decarbonisation. The company has more than trebled in size over the past two years and is already generating annual turnover of over £1 million in genuine sales. A fundraising process is currently underway seeking £15 million to help 6000 vehicles start taking advantage of ULEMCo’s dual-fuel hydrogen technology by 2030. To highlight the savings available, major customer Aberdeen City Council has been using a dual-fuel converted road sweeper since the start of 2022:
“We don’t change the base engine, so both the performance and operational reliability of a converted vehicle is assured; it will continue to run on diesel if no hydrogen is available,” says Amanda Lyne. “By using existing engine technology, the cost of becoming hydrogenenabled is minimal in comparison to other low-emission options, providing a great first step in achieving substantial emissions reduction, today.”
Talk to one of our hydrogen experts and let Parker meet your on-board hydrogen challenge
As a source of clean energy, hydrogen is making a great contribution to a more sustainable future. However, it can embrittle poor-quality steel materials, leading to unexpected component failures. This article looks at how materials certificates can protect OEMs from such problems.
Hydrogen is highly flammable – more so than regular fuel – and is harder to contain than oil due to its small particle size which brings understandable safety concerns. Fittings used in Hydrogen production, Hydrogen fuel cells and refueling stations must meet key performance criteria to ensure safety, reliability, and performance in application.
White Paper
We focus on supporting our customers through every step of their bonding process. Our teams will go on-site for technical service, troubleshooting and process optimization.
Video
Learn how Parker A-LOK® double ferrule fittings are EC-79 Certified for use on-board hydrogen powered vehicles
Brochure
An overview of Parker fluid system technology for Hydrogen powered vehicles
Brochure
Components and systems manufactured by Parker for use with gaseous and liquid Hydrogen in infrastructure and on-vehicle applications
1005 A Cleaner Way
Huntsville, AL 35805
Tel: 256.881.2040
Riverside Road
Barnstaple EX31 1NP
United Kingdom
Tel. 0044 1271 313131