DustHog dust collectors are an important investment that impacts air pollution control and the health of your employees. Whether the process is intermittent or heavy duty, we offer many collectors to fit your needs, ceiling-mount, downward flow, plug-n-play, cross-ventilation, and more.
SmogHog delivers ESP and Media Mist technologies so you get the right solution for your unique application. The decision is easy after you understand how this equipment is built and works. Local authorized Parker representatives and our application engineers will analyze your operation.
Eliminate smoke and odors caused by kitchen emissions with SmogHog® PSG air cleaning systems. SmogHog, a well-known name in the commercial kitchen exhaust and air cleaning industry solves fumes and saves you money.
Smokeeter, most commonly used in bars, restaurants, bowling alleys, office buildings, and other public facilities, uses Electrostatic Precipitator (ESP) technology to remove contaminants like dust, pollen, bacteria, fungi, smoke, and viruses far better than competitors.
Want more details about our industrial dust and mist collectors? We've gathered the information you need.
Register your product today to ensure your warranty and help with customer support.
Dust collectors are designed to capture and filter out solid particulates, such as dust and other larger airborne contaminants, from the air in industrial environments. They are often used in woodworking, metalworking, and other processes that generate a lot of dust. Dust collectors work by using a high-powered fan to create a vacuum that pulls air (and the dust it carries) into the system, where it's then filtered out. The clean air is then released back into the workspace, and the captured dust is disposed of.
Mist collectors, on the other hand, are designed to capture and filter out liquid particles or aerosols from the air. These are typically used in environments where processes generate a lot of mist or smoke, such as machining operations that use coolant or oil-based lubricants. The mist collector works by pulling the contaminated air into the system, where the mist particles are captured on a filter or through other means such as electrostatic precipitation or centrifugal separation. The filtered air is then released back into the workspace, and the collected mist is either disposed of or recycled, depending on the system and the nature of the mist.
The Occupational Safety and Health Administration (OSHA) sets forth regulations and guidelines to ensure workplace safety and health, including the management of dust in the workplace. Dust collection systems are crucial in many industries to control and minimize the exposure of workers to hazardous dust. The specific OSHA requirements for dust collection can vary depending on the type of dust (e.g., wood, metal, chemical) and the industry. For the most current information, visit the official OSHA website.
Dust collectors are critical for maintaining a healthy work environment, protecting workers from harmful dust, and complying with environmental regulations. The basic working principle of industrial dust collectors involves several key steps:
While sometimes these descriptions are used interchangeably, dust extractors are more suited for direct source capture and mobility, especially for fine particles and smaller workspaces. In contrast, dust collectors are designed for larger-scale operations requiring high-volume dust collection from multiple sources.
Sizing a mist collector is a nuanced process that requires a thorough understanding of your operational needs, the properties of the mist generated, and the specifics of your workspace. Accurate sizing is crucial for efficient operation, compliance with regulations, and ensuring a clean, safe work environment for workers.
Mist collectors, also known as mist eliminators or mist extractors, are devices designed to remove or collect mist or fine droplets of fluid from the air. These fluids can include oil, water, coolant, or other liquids that are used or generated in industrial processes.
The purpose of mist collectors is to improve air quality, protect worker health, enhance safety, and ensure compliance with environmental regulations. They are commonly used in industrial manufacturing settings, such as metalworking, machining, chemical processing, and food processing facilities.
Mist collectors can be installed directly on machines that generate mist or as central systems that serve multiple sources in a facility. They not only help in maintaining a cleaner and safer work environment but also contribute to the recapture of valuable fluids that can be recycled and reused in the process, thereby reducing waste and potentially saving money.
United Air Specialists was part of CLARCOR Industrial Air. CLARCOR joined Parker’s Filtration Group in 2017 and brought proprietary media, industrial and process filtration products, and technologies, as well as a broad portfolio of replacement filters. United Air Specialists along with the DustHog®, SmogHog®, and BHA® brands can be found here in the Industrial Gas Filtration and Generation division.