OVERLAND PARK, KS, August 08, 2019 - The Industrial Gas Filtration and Generation Division of Parker Hannifin Corporation, the global leader in motion and control technologies, today announced the launch of an important new patent for the metalworking industry. The patent is designed to optimize drainage within the SmogHog® SHM self-contained media mist collector and provide best in class particulate removal efficiency and long filter life using state of art coalescing filter media technology.
The patent includes an area that supports the industrial filter elements, sealing the upper and lower plates of the filter, a liquid collection area, and a reservoir in the base section to drain away the liquid that coalesces during operation. Suspended liquids collect and coalesce on the fiber structure of the filter, the droplet size grows, and gravity drains the contaminants from the airstream and out of the filter into the collection area.
The media used within this proprietary design provides an open 3-D depth matrix structure that separates the liquid droplets from the airstream, into three airflow paths, radial, axial and helical, removing 99% of contaminants. Air passes directly through the thickness of the media impacting the fiber structure removing the contaminant, the media then forces a great amount of the airflow to take a stair-step path improving particle removal and the third path creates a corkscrew pattern that increases dwell time and resulting particle capture.
“This invention joins many other industry-leading patents we have brought to industrial filtration,” said Jeff Canfield, product development engineer, Industrial Air Filtration of Parker Hannifin, “Preveil®, PulsePleats®, and ProTura®, to name a few. This media technology is built into a tubular arrangement, this coupled with the SHM three-stage filtration process our customers will see a 99% reduction in mist concentration.”
The three-stage process includes a mist-stop pre-filter, a fine fiber, aluminum mesh pre-filter that reduces mist concentration and coarse contaminants, a primary filter engineered with PEACH® coalescing cartridges and the final stage, a safety after-filter available in ASHRAE 95% oil mist rates filter or HEPA configurations.
Learn more at www.parker.com/airquality or call us +1 800-821-2222.
This patent is known as U.S. Patent US-2018-0339255-A1.
About Industrial Gas Filtration and Generation (IGFG) Division
Parker Hannifin’s IGFG Division protects and purifies using diverse solutions engineered for the customer's unique application. We are the filtration resource for customers backed by state-of-the-art labs and advanced filtration research, world-class manufacturing processes and application engineering experience for any filtration challenge.
About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than 100 years the company has engineered the success of its customers in a wide range of diversified industrial and aerospace markets. Learn more at www.parker.com or @parkerhannifin.
Lori Dowd
Marketing Communications Director
11501 Outlook Street, Suite 100
Overland Park, Kansas 66211
1-913-374-3162