The custom or replacement filters for OEM brand dust collectors offer design improvements that provide customers longer filter life and lower pressure drop
OVERLAND PARK, Kan., October 12, 2021 – The Industrial Gas Filtration and Generation Division of Parker Hannifin Corporation, the global leader in motion and control technologies, has introduced two new aftermarket cartridge filters. Parker designs filters to meet special applications and manufactures aftermarket filters for most OEM dust collection equipment with design improvements to help customers improve their bottom line.
The division’s newest development is a replacement cartridge filter for an OEM brand dust collection system. The key advantage to this filter is the enhanced, more conventional design. This filter is constructed without the inner conical filter the OEM included, creating a greater pleat depth. For enhanced sealing, the filter has a wider gasket contact area than the OEM filter. To resist bowing, the replacement cartridge is constructed with a stiffer, and heavier gauge sheet metal top pan and the robust filter design also includes a galvanized expanded metalcore, urethane potting compound and four 1” wide reinforcement straps.
Another notable feature of this pulse-jet cartridge filter is that it can directly interchange with the OEM filter without any required modification of the dust collector. This enables the replacement cartridge to be compatible for use in any application currently using the OEM filter with similar media.
“This replacement cartridge was engineered to solve problems customers experience with the OEM brand filter. With greater pleat depth and proven design enhancements, beta site customers report lower pressure drop and longer filter life,” said Jeff Canfield, senior product engineer, Industrial Gas Filtration and Generation Division.
Parker has developed dozens of OEM brand competitive fit filters, including a 52” cartridge using a continuous, full-height pleatpack rather than the original configuration of stacking and joining two 26” tall cartridges. For customers, this means less potential for leaks, no wasted media at the connection of the two sections and less labor and materials needed to make one full-height pleatpack. Parker delivers improved performance - ultimately leading to a safer, cleaner and lower maintenance work environment.
For more information or to discuss the right replacement filter for your system, please visit Parker.com/BHA.
About Industrial Gas Filtration and Generation (IGFG) Division
Parker Hannifin’s IGFG Division protects and purifies using diverse solutions engineered for the customer’s unique application. We are the filtration resource for customers backed by state-of-the-art labs and advanced filtration research, world-class manufacturing processes, and application engineering experience for any filtration challenge.
About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
Lori Dowd
Marketing Communications Director
11501 Outlook Street, Suite 100
Overland Park, Kansas 66211
1-913-374-3162