Parker Hydrogen Refueling Filters - Industrial Gas Filtration & Generation Division | Regional English sites

New filters maximize equipment uptime, decrease maintenance costs and ensure safe operations

HAVERHILL, MA., April 14, 2025 – The Industrial Gas Filtration & Generation Division of Parker Hannifin Corporation, the global leader in motion and control technologies, announced the release of its new high-pressure filter models for gaseous hydrogen, designed to meet the robust demands and stringent requirements for cleanliness and efficiency.

Engineered with advanced filtration media technology, these filters effectively remove contaminants such as moisture and particulates to ensure the hydrogen used in fuel cells is of the highest quality. By providing reliable and robust solutions, Parker is committed to supporting the hydrogen economy by providing reliable and robust solutions to enable a sustainable energy future.

These are the first in a new line of filters created specifically for use with hydrogen gas. The design offers a familiar configuration of an in-line mounted style which features a head, bowl and high efficiency rated element. The filter also utilizes 316 stainless steel to reduce risk of hydrogen embrittlement, as well as multiple port type options for a wide range of application coverage. These filters have a pressure safety factor of 3.8, which is above the industry standard safety factor of 2.5, and are listed with Canadian Registration Numbers (CRN) in all provinces. Additionally, they carry CE Marking in accordance with the Pressure Equipment Directive 2014/68/EU.

The RL0700, RM0700 and upcoming RH1000 models provide critical protection as the last line of defense from contamination. The filter will minimize downtime by eliminating risk of damage to equipment and sensitive components. These filters reduce the chance of aerosols and particulate contamination carryover during the fuel dispensing process.

“We designed the R Series hydrogen refueling filters with multiple inlet/outlet port options and flow rate choices for maximum flexibility,” said John D’Antonio, engineering supervisor for Parker’s Industrial Gas Filtration & Generation Division. “They deliver clean hydrogen to the vehicle that meets SAE J2719 cleanliness protocols”.

The R Series filters are manufactured in Haverhill, Massachusetts and continue Parker’s long history of improving safety and sustainability in alternative fuels. The RL0700 and RM0700 filters are available for purchase today, and the RH1000 will be available in May 2025. Parker’s teams are dedicated to delivering best-in-class quality and customer service without undue delay.

Learn more about the Hydrogen Refueling Filter at www.parker.com/h2filter.

About Parker Hannifin

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.

MEDIA CONTACTS

Mike Cieniawa,
Product Sales Manager
Industrial Gas Filtration & Generation Division
Phone (978) 478-2026
michael.cieniawa@parker.com