In recent years, high-pressure nitrogen or oxide-free, assist-gas cutting has won favor from job shops and OEMs because of the cut quality achieved when inert gas is used in the laser cutting process. Parts processed using high-pressure nitrogen are produced virtually burr-free and do not need secondary grinding operations. Because there is no oxide layer, the resultant edge is a bright, milled quality that makes for better welds.
As laser cutting system capabilities grow, applications for high-pressure nitrogen cutting also expand. Once considered most suitable for stainless steel and aluminum, high-pressure nitrogen cutting is now being applied to light gauge mild steel in applications where an oxide layer presents a concern and part quality is essential. In this overview, we will examine:
1. High-pressure assist-gas cutting process
2. Advantages of high-pressure laser cutting with nitrogen in stainless steel and mild steel applications
3. Costs of using nitrogen as an assist gas
Nitrogen as an Assist Gas for High-Pressure Nitrogen Cutting
Nitrogen is the most commonly used inert gas. Other inert gases used in laser cutting can include argon and helium. Because of nitrogen's stability, it is commonly used as a high-pressure assist gas, while argon and helium are used for more specialized material-specific applications. Benefits include:
The absence of an oxide layer also makes the nitrogen-processed part weld-ready. In contrast, stainless steel parts cut using oxygen-assist gas must be ground to remove the oxide layer before welding. The resulting weld will be structurally inferior due to porosity if the oxide layer is not removed.
High-pressure nitrogen also helps cool the part, minimizing heat penetration or the size of the heat-affected zone (HAZ). This is particularly apparent in thick stainless steel from 4.7 to 13 mm, where the HAZ is most often measured in tens of thousandths of an inch instead of cutting with oxygen assist, where the HAZ may be as much as 10% of the material's thickness.
The technique employed when high-pressure assist cutting with nitrogen differs from cutting with oxygen-assist gas. When high-pressure cutting is employed, the laser's focal point setting must be adjusted into the bottom 10 to 15% of the material. The focal point is set at the part's surface when cutting with oxygen. Driving the focus deeper into the part makes the resultant kerf wider and allows for the optimum ejection of molten material. The wider kerf also allows a higher gas volume to be pushed into the kerf, creating an optimum shield for the edge.
Nitrogen shields cut edges from oxygen, so an additional process to remove an oxide is unnecessary. In addition, high-pressure inert gas cutting requires using a larger nozzle orifice, 1.5 to 2.5 times larger than nozzles used for oxygen-assist cutting. This allows for maximizing the assist gas column's pressure and volume. The nozzle's internal geometry is designed to allow the assist gas column to attain a higher velocity.