Cement companies face extremely tough compliance and regulation requirements in addition to manufacturing issues resulting from fine, abrasive dust and older filtration equipment.
Common baghouse and filtration challenges we tackle include fine particulate emissions that lead to bleedthrough, aggressive designs and high filtration velocities that can cause filter failure, high differential pressure/loss of airflow, poor cleaning, and extra drag across filters from primary dustcake, and abrasion failure.
Manufacturing facilities globally are running at capacity. However, the demand for all finished plastics remains high in all markets. Plastics processing covers a broad range of operations. The last thing you need is your generators or filtration systems to contribute to unscheduled downtime and lost production.
We can help you keep employees safe, eliminate outside vendor challenges, and improve product quality. Our nitrogen generators, dust and mist collectors, and industrial filters are used in a wide range of processing applications, from blanketing, flue gas sampling, to weighing, batching, blending, mixing (mulling), drying, burning, calcining, hydrating, sizing, screening, and packaging.
A vast range of manufacturing processes are part of the food and beverage industries. Strict hygiene regulations and demanding requirements mean most areas require filtration, particulate collection, and gas generation.
We design solutions to ensure your methods do not risk employees' health and safety, eliminate product cross-contamination, and equipment problems. Clean and pure ingredients contribute to the quality of the end product, whether it's potato chips, pinot grigio, or sugar. The result is higher yields, fresher products, and satisfied customers.
Competitive manufacturers focus on engineering excellence, productivity, quality, and reducing operating costs. There are many considerations to ensure efficient, cost-effective production that is safe for the environment inside and outside your facilities.
We are the industry-leading dust and mist filtration, desiccant and refrigerated dryers, nitrogen generation, and process cooling systems manufacturer. We deliver cost and energy-saving solutions to maximize your up-time, keep the air clean of harmful pollutants, and increase your bottom line.
Collaborating with medical and analytical device OEMs, we work with customers to deliver inventive gas generation equipment subsystems that break new ground. As a result, leading medical equipment manufacturers and health institutions worldwide rely on our solutions to operate analytical instrumentation and prevent hospital-acquired infections.
If you want to provide consistent gas quality and pressure that improves stability and ensures greater reproducibility of results while minimizing safety risks to your employees, contact us.
Air quality is a significant priority. The particles released during the metals and machining processes are dangerous, and you need dust collection equipment and baghouse filters that you can trust.
Extensive dust properties must be evaluated and understood for the filtration system to provide high efficiency, extended filter life, and environmental protection. Examples of properties include particle size, density, moisture content, stickiness/flowability, temperature, reactivity, toxicity, and flammability. A wide array of applications, and no matter which area you are in, we have the expertise to be a valuable partner.
You need to keep your pipeline full, and we can help by ensuring your production equipment is operating efficiently during upstream extraction phases and protecting product purity as oil and gas pass through the midstream and downstream phases of product transport and distribution.
Designed to control, improve and stabilize your processes, our filters, and nitrogen generators deliver flexibility and feed air options for both onshore and offshore applications.
Pharmaceutical processing is one of the highest-regulated industries and we are here with solutions to help. Almost every process in the manufacturing of pharmaceuticals generates some dust; granulating, grinding, drying, mixing, pressing, coating, as well as during the cleaning of the equipment and moving of materials, dust will be created.
We can help ensure your facility doesn't threaten your employees' health and that your products remain pure for your customers. Leading pharmaceutical manufacturers know our dust collection equipment and baghouse filters are reliable and provide the highest level of filtration. We help you put the focus back on engineering excellence, productivity, quality, and reducing operating costs so you can keep your plant running profitably.
As a retail developer, building owner, tenant, architect, or engineer, you know how much a restaurant can add to the value of your venue. But you’re also well aware of the environmental issues that can result from annoying smoke and greasy odors emitting from kitchens and the headaches that result from designing them.
We understand spaces can be tight, and meeting air quality environmental standards at the federal, state, and local levels is essential. As a world leader in air pollution control, we have the cooking ventilation expertise and the architectural perspective required to ensure you have an emissions system that allows you to run your industrial or commercial kitchen without worrying about air quality.