Selecting the Right Motor - Hydraulic Pump and Power Systems Division | Parker US

Hydraulics

Selecting the Right Motor >

Essential Criteria for Selecting the Right Motor for your Hydraulic Application

Hydraulic System

 

Introduction

The ideal in hydraulic system design is to match overall efficiencies to the application performance expectation. This requires the designer to first match the motor, then the pump to a specific system performance expectation. Whether the requirement is to do something within a specific time frame, or in handling a given amount of load, the design of the entire system will change depending on the motor selected.

A hydraulic motor is a hydraulic actuator that, when properly connected into a hydraulic system, will produce a rotary actuation. This can be unidirectional or bidirectional depending on the system design. Motors are similar in design to pumps only where a pump takes a rotary actuation to move hydraulic fluid out of the unit, whereas a motor will take flow into itself and put out a rotary actuation.

The motor selection comes first in the process because application design best practices require that you start with the load requirement, then work back to the prime mover—the pump that will put the fluid power into the motor selected to deliver the performance goal.

Each motor type—gear, vane, in-line piston, bent-axis piston and radial piston—has a specific performance profile. So, knowing the application performance requirement and which motor type best meets the objective is the first step. Then it’s necessary to evaluate the design advantages of your motor options along with the degree of complexity you want for the overall system.

In the end, it all goes back to the application’s performance expectations. Some have severe duty cycles, while others do not. If, for example, you consider running a low-efficiency, lighter-duty motor into a higher-duty cycle application, the life of the motor will be less than the life of a higher-duty cycle motor that is designed to operate in those types of environments. It is important to understand what operating pressures and flows are required for the motor selected to achieve the application performance expectations.

Each motor type has its own set of applications where they are a better choice than others. For example, if a small gear motor designed to operate at a max of 3,000 psi and 1,000 rpm is put into an application that requires it to run consistently at 3,000 psi and 1,000 rpm, the motor will be running in a “corner” overstressed condition and have a reduced life—even though it is technically within its ratings. The better motor choice would be a motor with higher ratings that will live longer in the application. Granted, there is a greater cost in going with a higher rated motor. The final decision always will depend on what is required in terms of application performance and motor life versus where you want to be with cost.

How Motors Are Rated 

Motors are rated by displacement, with displacement defined as the volume of fluid that it takes to rotate the shaft of the motor once. The common rating units are cubic inches per revolution (CIR), or cubic centimeters per revolution (CCR).

Motors are also rated by torque—the amount of twisting force the motor can deliver. The common measurements of torque are inch-pounds (in.-lb) and Newton-meters (Nm). The torque of a motor is a function of motor displacement and system pressure.

Starting torque is the torque the motor can generate to turn a load when starting from a stop. In general, starting toque is the lowest torque rating of a hydraulic motor due to inefficiencies.

Stall torque is the maximum torque the motor will generate before it stops rotating. Sometimes this is also referred to as running torque. The rotational speed of the motor shaft is measured in units of rotations per minute (rpm). Motor speed is a function of hydraulic input flow and motor displacement.

Common Motor Classes and Type 

Generally, hydraulic motors are placed into one of two classifications: high speed, low torque (HSLT) or low speed, high torque (LSHT).

Gear Motors

Gear motors come in two varieties—the gerotor/geroller or orbital and external spur gear designs. Orbital styles are classified as LSHT motors; however, some do exist with the HSLT classification. They consist of a matched gear set enclosed in a housing. When hydraulic fluid is moved into the motor, it causes the gears to rotate. One of the gears is connected to the motor output shaft, which produces the motor’s rotary motion.

Key features include:

• low weight and size

• medium pressures

• low cost

• wide range of speeds

• wide temperature range

• simple design

• wide viscosity range

Applications include mobile hydraulics, agricultural machinery to drive conveyor belts, dispersion plates, screw conveyors or fans. Their biggest drawback is that they have a higher noise level.

Vane Motors 

Vane motors are typically classified as HSLT units. However, larger displacements will fall into the LSHT range. Hydraulic fluid enters the motor and is applied to a rectangular vane, which slides into and out of the center rotor. This center rotor is connected to the main output shaft. The fluid being applied to the vane causes the output shaft to rotate.

Parker’s vane motors feature a balanced design where the inlet and outlet ports of the motor are applied to sections of the vane cartridge that are 180° apart from each other to ensure that the hydraulic forces are always in balance inside the motor.

Key features include:

• low noise level

• low flow pulsation

• medium pressure

• high torque at low speeds

• simple design

• easy versatility

• vertical installation friendly

They are used in both industrial applications, such as screw-drive and injection molding, and mobile applications such as agricultural machinery.

Piston Motors

Piston motors come in a variety of designs with both LSHT and HSLT classifications.

In-line piston motors are classified as HSLT. Hydraulic fluid enters the motor and is applied to a series of pistons inside a cylinder barrel. The pistons are pressed against a swash plate, which is at an angle. The pistons push against this angle, which causes the rotation of the swash plate that is mechanically connected to the output shaft of the motor. The swash plate can be a fixed or variable angle. Variable angle motors can have their displacements adjusted between a maximum and minimum setting. The command signals to change the displacement can be electrical, hydraulic or a combination of both.

Bent-axis piston motors are classified as HSLT. They are similar to inline motors except that the piston barrel is at an angle in relation to the swash plate. Hydraulic fluid enters the motor and is applied to the pistons, which are contained in a cylinder barrel. The pistons are at an angle to the drive shaft, which means that the piston will rotate the shaft as fluid enters the motor.

They can be both fixed and variable displacement. In a variable-displacement bent-axis motor, the cylinder barrel is rotated between maximum and minimum displacements. The command signals to change the displacement can be electrical, hydraulic or a combination of both.

They are best known for high performance, high pressures, high speeds and volumetric mechanical efficiencies in the 97 to 98% range. They also offer quick reaction and precise control. These motors are suitable for applications that require a significant amount of power. 

They are used to drive mobile and construction equipment, winches, ship-cranes and all kinds of heavy-duty hydraulic equipment for off shore and onshore operations.

Key features of in-line and bent-axis piston motors:

• higher speeds

• higher efficiencies

• can be fixed or variable displacement

• multiple controls to adjust displacement

• wide range of speeds

• high power density

Radial Piston Motors

Radial piston motors are LSHT classified. These motors are designed with pistons arranged perpendicular to the output shaft. Typically, the pistons will ride against a cam, which is mechanically connected to the output shaft. The pistons will force the cam to rotate as hydraulic fluid enters the motor.

These motors are capable of producing high torques at low speeds, down to half a revolution per minute.

Applications include caterpillar drives of dragline excavators, cranes, winches and ground drilling equipment.

In general, these motors are fixed displacement. However, some versions will allow for variable displacement. They accomplish this by limiting the number of pistons that can receive hydraulic fluid. Other versions change the internal geometry of the cam the pistons are acting against.

Key features of radial piston motors: 

• higher output torques

• lower output speed

• smoother output speed at low speeds (no “cogging”)

• simplification of system design by reducing or eliminating gearboxes or other mechanical ratios that would need to be used in the system

Motor Selection Consideration

All of the following questions are important to answer when selecting a hydraulic motor:

• What are the performance needs of the application?

• What is the load and amount of break away and running torque needed?

• What is the shaft speed and horsepower?

• What is the operating pressure and flow?

• Is displacement fixed or variable?

• What is the operating temperature?

• Is there any leakage potential?

• What noise level can the application handle?

• How reliable is the motor design?

• What type of controls will be used—mechanical or electronic?

• Is ease of installation critical?

• Is ease of maintenance necessary?

• What is the bearing type and expected life?

• What is the expected motor life?

• Is it open or closed loop?

• What kind of contamination potential is there?

• What certifications and approvals are needed?

Proper hydraulic motor selection starts with the expected performance required by the application, then works back to the prime mover—the pump. Then it is necessary to evaluate the cost of your motor options along with the degree of complexity you want for the overall system.

Download the Guide: 

Download the Success Story: 

 Download