Parker Introduces eConfigurator for Power Units - Hydraulic Pump and Power Systems Division | Regional English sites
Parker engineering expertise at your fingertips – allowing easy customizations to a hydraulic pump solution tailored to an end user’s unique needs                                                                                                                                                                                                                                                                                                                             

MARYSVILLE, OHIO, July 27, 2023 - The Hydraulic Pump and Power Systems (HPS) Division of Parker Hannifin Corporation, the global leader in motion and control technologies, today announced a new online configuration tool for the following product series:

-          Compact Hydraulic Power Unit - 108 Series

-          Compact Hydraulic Power Unit – 165 Series

-          Compact Hydraulic Power Unit – 550 Series

-          D-PAK Fixed Displacement Hydraulic Power Units

-          H-PAK Fixed Displacement Hydraulic Power Units

-          V-PAK Fixed Displacement Hydraulic Power Units 

The eConfigurator tool will streamline a user’s online configuration with a convenient embedded tool view, including model-based dimensioning and an extended product summary in one location.

eConfigurator features include:

An additional 17 engineering specifications to conveniently view and confirm dimensions and detailed specs prior to downloading a CAD file, enabling an easier specification process.

An enhanced model code to directly specify additional product settings and options, such as displacement and pressure settings. These features are communicated through an improved, comprehensive model code, resulting in more precise product selections and ultimately a quicker specification process.

A convenient workflow method through the share configuration function, which allows the user to generate and send via email a unique URL of the configuration. This feature is meant to enhance collaboration between stakeholders to further streamline requirements and shorten the specification and purchase phases.

Online quoting providing the user a way to electronically send a detailed product configuration for a pricing and delivery quote.    

Learn more about the new eConfigurator at: https://discover.parker.com/neweconfig

About Hydraulic Pump and Power Systems Division
A global technology leader, the Parker Hydraulic Pump and Power Systems Division brings nearly a century of combined experience. Our division is the result of the Parker piston pump business’s acquisition of Denison Hydraulics in 2004 and our mergers with the Parker Oildyne Division and the Parker Electromechanical Drives Division’s (EMD) electric motors and gearboxes. Since before WWII, Denison products have been excelling in military test stand and shipboard hydraulic applications. This acquisition allowed us to enhance the design, manufacturing and application of piston products in both open- and closed-circuit applications. With the addition of Oildyne, we have extended our offering to include the quality compact hydraulic products and systems the division has been pioneering since 1955. Like the miniature piston pumps Oildyne manufactures, it’s been a smart fit. With the Summer 2021 addition of electric motors and gearboxes from Parker’s EMD, HPS is focused on the future of both electric and hydraulics solutions for a wide variety of applications including trucks, buses, and construction equipment vehicles.                                                                                                                                                                                                                                                                                                                                                                                                             


About Parker

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.

###

MEDIA CONTACTS

Larissa Livingston

Digital Marketing Manager

14249 Industrial Parkway

Marysville, OH 43040

937.644.4490