Parker Showcases Its Configured ePumps at IFPE 2023 - Hydraulic Pump and Power Systems Division | Regional English sites
High Efficiency and Superior Reliability at a Low Installation Cost                                                                                                                                                                                                                                                                                                                               

MARYSVILLE, OHIO, March 09, 2023 - The Hydraulic Pump and Power Systems Division of Parker Hannifin Corporation, the global leader in motion and control technologies, has announced it will feature its configured ePumps, the EHP Series, at the International Fluid Power Exposition (IFPE) at the Las Vegas Convention Center in Las Vega, NV from March 14 - 18, 2023.


Parker's EHP Series Configured ePumps consist of an electric motor, directly coupled to a hydraulic pump, and can be easily controlled by a GVI Series high performance mobile hardened inverter. Parker's global expertise in hydraulic pump and electric motor technologies is combined into the EHP Series, creating an optimized and customizable system for hybrid electric and fully electric mobile work function and auxiliary applications. The EHP Series consists of a wide range of motor and pump combinations adaptive to every battery pack, resulting in greater flexibility.


These combinations include:
GVM Electric Motor and P1M Piston Pump
GVM Electric Motor and T7 Vane Pump
GVM Electric Motor and F11/F12 Bent Axis Pump
GVM Electric Motor and PGP Gear Pump


“Our Configured ePumps provide a low installation cost, high efficiency, while still maintaining superior reliability in the most demanding applications. Parker's EHP Series Configured ePumps also offer customers a simplified sourcing option through its tested and provide multi-technology solution available from one supplier," said Andrew Cailteux, Business Development Manager, Parker's Hydraulic Pump and Power Systems.


Learn more about Parker's Configured ePumps, EHP Series: https://discover.parker.com/EHP


About Hydraulic Pump and Power Systems Division
A global technology leader, the Parker Hydraulic Pump and Power Systems Division brings nearly a century of combined experience. Our division is the result of the Parker piston pump business’s acquisition of Denison Hydraulics in 2004 and our mergers with the Parker Oildyne Division and the Parker Electromechanical Drives Division’s (EMD) electric motors and gearboxes. Since before WWII, Denison products have been excelling in military test stand and shipboard hydraulic applications. This acquisition allowed us to enhance the design, manufacturing and application of piston products in both open- and closed-circuit applications. With the addition of Oildyne, we have extended our offering to include the quality compact hydraulic products and systems the division has been pioneering since 1955. Like the miniature piston pumps Oildyne manufactures, it’s been a smart fit. With the Summer 2021 addition of electric motors and gearboxes from Parker’s EMD, HPS is focused on the future of both electric and hydraulics solutions for a wide variety of applications including trucks, buses, and construction equipment vehicles.                                                                                                                                                                                                                                                                                                                                                                                                             


About Parker

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.

###

MEDIA CONTACTS

Larissa Livingston

Digital Marketing Manager

14249 Industrial Parkway

Marysville, OH 43040

937.644.4490