All it takes is one costly outbreak from any number of common diseases to significantly impact your swine or poultry population. Investing in Parker’s high-quality air pathogen barrier filters can protect your livestock from catastrophic effects of various animal infectious diseases.
Poultry and livestock diseases like the ongoing highly pathogenic avian influenza inflict a substantial economic toll on producers, impacting both direct and indirect costs. Direct costs include the immediate loss of animals, decreased production efficiency, and the expenses associated with veterinary care and disease containment measures. Indirect costs are equally significant, encompassing disruptions in the supply chain, reduced market access, and the long-term impact on consumer confidence and demand. The economic repercussions of these diseases underscore the critical need for effective prevention and management strategies to safeguard farms.
For over 50 years, Parker has been improving the quality of air around the world with trusted products that define excellence. Our strong relationships with agricultural producers have enabled us to understand their unique air quality challenges and tailor filtration solutions to meet their requirements. You can expect Parker to stay at the forefront of technological advancements, continuously innovating to deliver the highest levels of quality, efficiency, and value for our agricultural customers who produce food essential for human survival.
By installing Parker’s high-quality pathogen barrier final filters, poultry farmers have reported significant improvements at their production facilities. On average, bird mortality decreased by 30%, demonstrating measurable population consistencies. With improved air quality across multiple facilities, disease outbreaks have lessened considerably.
You’ll find Parker’s air filtration products on local farms and commercial production facilities across the globe. There are approximately 600,000 Parker Log 9 or Pur Ag® V-Bank air filters in use in agricultural buildings today.
Designed with extreme durability in mind, XTREME+Plus® MERV 8 standard and high-capacity filters offer the best self-supported pleat (SSP) performance on the market. XTREME+Plus achieves extremely low pressure drop and industry-leading dust holding capacity. Their robust construction will save time and money previously wasted on damaged wire-backed filters. With no metal that can warp or deform, a moisture-resistant beverage board frame, and 100% synthetic media, XTREME+Plus filters maintain their integrity even in wet or humid conditions.
By installing Parker’s Pur Ag® V-Bank pathogen barrier final filters, you can trap airborne viruses before they enter your facilities. Designed specifically for agriculture buildings, Pur Ag V-Bank filters are MERV 15-rated and 12˝ deep. PurAg V-Bank filters install easily into the filter grid frame, eave housings, attic housings, or metal filter frame. Tested to ASHRAE 52.
Parker’s Pur Ag® SlimBox filters help producers reduce risk, improve air quality, and increase profits at their facilities. The patented filter is MERV 16-rated and 6˝ deep with Log 9 viral efficiency that provides industry-leading airflow at low resistance. SlimBox filters feature 100% synthetic, moisture-resistant, gradient density media that will not support microbial growth. They install easily into the filter grid frame, eave housings, attic housings, or metal filter frame.
Talk to Parker about air filtration
Follow us at:
Parker's Filtration Technology Blog