Sipiol UV Dielectric Coatings for Battery Packs - Elastomer Process Materials Division | Parker US
Man inspecting battery pack

Sipiol UV is a UV-cured, VOC-Free, 100% solids, dielectric coating that cures in seconds that has superior adhesion to metals and plastics. Sipiol UV coatings was specifically formulated for edge coverage and flexibility to prevent catastrophic battery fires. The strong adhesion and flexibility blends itself to many applications in the battery assembly.

Webinar On-Demand

Dielectric Coating for EV Battery Packs

What We Cover: 

  • Sipiol UV offers improve edge coverage and provides dielectric protection where existing solutions may fail

  • How this coating can improve bonding strength to other components in the battery pack

  • Sipiol UV can increase throughput and offers quick handling strength due to the rapid cure

  • 100% VOC free and environmentally friendly

Webinar Dielectric Coating for EV Battery Packs

PET Replacement with Dielectric Coating

Sipiol UV can replace PET on Cylindrical and Prismatic Cells which will eliminate delamination at corners and seams and has superior adhesion to battery cells. Sipiol UV will not de-bond or delaminate during use. Our dielectric paint contains unique properties with good coverage and high flexibility, allowing it to be applied to complex geometries where other battery coatings or tapes may fail. Production time can be reduced with the rapid cure time in a matter of seconds, not hours. Note: the delamination with the sharp corner and maintaining isolation is vital to safety in high voltage batteries and even more important as density energy increases.  

How Parker Innovated Sipiol UV to Solve Battery Delamination Issues

Watch as Parker collaborates closely with a leading battery manufacturer to address a critical issue: the delamination caused by traditional PE tape at the edges of batteries. 

Dielectric EV Battery Coating

How Does Sipiol UV Work?

Our chemistry can cure rapidly when exposed to the appropriate wavelength and the intensity of light. When UV light is applied to the liquid coating, the photoinitiator produces free radicals which begin the chain reaction when polymerizing the liquid monomers into a cross linked and cured coating.

UV light cures
EV Battery and Motor

Whitepaper

With the growth and development of battery pack technologies, manufacturers of electric vehicles (EV) place greater emphasis on pack design optimization, seeking more compact solutions to improve energy density and reduce cost. Dielectric protection is critical in the assembly of high-voltage battery packs. Manufacturers often apply dielectric materials to the battery cells, cooling plates and adjacent components.

Several types of dielectric materials exist on the market today. Four of them will be discussed, tested, and compared in this paper.

How to Apply Sipiol UV

Sipiol UV has excellent edge coverage without delamination when applied to battery packs. Preventing delamination and maintaining electrical isolation is Vitol to safety in high voltage batteries and even more important as energy density is increased. Watch this video to see how Sipiol UV is applied and the safety tests the material goes through.

How to apply Sipiol UV Video

Not sure which adhesive you need? Talk with one of our experts.

Call Us at 877-275-5673