Data centers and servers are vital infrastructure components, responsible for storing, communicating and transporting the massive amounts of information that are generated daily. These applications play a key role in everything from facilitating modern conveniences to ensuring mission-critical data exchanges and keeping them at peak performance with no downtime is a top organizational priority.
Due to the power and volume of electrical applications, high-frequency electromagnetic interference (EMI) shielding must be carefully and proactively managed. And as electronics get faster and more powerful, these considerations become more important than ever. High-powered devices are more likely to require an increased level of EMI shielding and are likely to generate a lot of heat, which can cause models to fail if the right precautions aren’t utilized.
Data centers must find ways to evolve with emerging technologies and utilize products and systems that can perform in these environments.
To ensure adequate EMI shielding for servers and data centers, there are several solutions that can be used. It’s important to find the right electrically conductive gasket for your application, and Parker Chomerics offers several options within our proven SOFT-SHIELD® product family.
One option within the Soft-Shield family is Fabric-over-foam (FoF) conductive gaskets. FoF provides a very economical solution for low-closure force electronic applications that require EMI shielding and electrical grounding. To create this - product, engineers start with a non-conductive low-density foam and then wrap conductive fabric around it. By combining the conductive properties of an electrically conductive fabric and the conformability of a foam core construction, the SOFT-SHIELD FoF product family ensures both high conductivity and high cycle reliability at an affordable price. FoF products offer a lot of engineering flexibility as well and can be custom designed to suit specific applications.
One FoF product that is ideal for most data center and server applications is SOFT-SHIELD 3500. These EMI shielding gaskets utilize a soft urethane foam core that is wrapped in a conductive nickel-plated copper fabric. The result is excellent compression set in low-closure force applications requiring high shielding effectiveness.
Another economical EMI shielding option for data centers and servers is conductive foam products. Conductive foam solutions from Parker Chomerics are unique in that they contain embedded silver-plated fibers verses traditional used conductive particles. Most conductive foams often lose their integrity when particles are added and subsequently won’t bounce back easily resulting in poor compression set. Instead of particles, we use fibers that run the length of the foam itself. These fibers maintain their contact from one side of the surface to the other, helping them maintain good electrical contact and good compression set.
SOFT-SHIELD 4850 conductive foam is an excellent choice to protect servers and data centers from the harmful impacts of EMI. This product contains silver-plated fibers that are embedded into low-density, open-cell urethane foam for stable electrical performance as well as superb conductivity with extremely short ground paths. SOFT-SHIELD 4850 also offers great design flexibility, coming in sheets that can be dye cut to fit many different applications.
Both SOFT-SHIELD 3500 and 4850 provide very low compression force because they are soft and allow for a large deflection range, which means they won’t damage fragile electrical components within applications. Additionally, both have high-temperature formulations which utilize a silicone foam for operating temperatures up to 125°C.
High-performing products can only do their jobs if they’re backed by a reliable manufacturing process. At Parker Chomerics, we take a global approach to manufacturing that is not solely reliant on a single manufacturing location. With multiple production centers across different countries, we can offer the same high-quality products from two or more locations, enabling flexibility, faster delivery, and efficient logistics. We’re proud to serve our customers with customized solutions that meet their specific requirements.
As electronics become more powerful, we’ll be ready to help data centers and servers manage the load. Parker Chomerics engineers are experts at 5G mmWave EMI shielding and other thermal solutions that keep base stations, towers, IT servers and more performing at their best to keep critical communications safely flowing.
Blog Post contributed by Jesse Hagar, Product Manager, Parker Chomerics.
Faster Electronic Performance with 5GmmWave EMI Shielding
EMI Shielding and Thermal Solutions for High Frequency 5G Applications
EMI Shielding for Powder Coated and Painted Enclosures with CHO-MASK II EMI Foil Tapes
On Demand Webinar: EMI Shielding and Thermal Interface Solutions for Telecommunications Applications
Parker Chomerics family of SOFT-SHIELD electromagnetic interference (EMI) shielding gaskets are designed for EMI shielding and grounding applications that do not require a weather seal.
Tell us a little bit about your problem and we'll do our best to come up with a cost effective, timely quote to help you get started.