Metal to Plastic Conversion for Automotive Applications - Chomerics Division | Parker US
Parker Image

Parker Chomerics

We're revolutionizing the automotive industry through our innovative metal to plastic lightweighting solutions. Our mission is to drive sustainability and efficiency in the production of both Electric Vehicles (EVs) and Internal Combustion Engine (ICE) vehicles.

Test Our Products for Your Project

Metal-to-Plastic Conversion Benefits for Automotive Engineers

For automotive engineers looking to reduce vehicle weight, metal-to-plastic conversion is a win-win. At the highest level, injection plastic molds are capable of producing multiples of millions of parts required for automotive programs with ease. Typically, a single tool can support a program for its entire life-cycle, meaning you only must go through the cost and design of tooling just once.

Parker Image

Access Port Covers for EV Cooling Systems

Meeting the Needs of Automotive OEMs with Collaborative Engineering Innovation

Plastic components provide a low-cost, space-saving solution, enabling Original Equipment Manufacturers (OEMs) to meet the integrated cooling requirements of high-torque electric motors. These products are backed by machine-based process monitoring, ensuring each manufacturing and assembly step is completed thoroughly and correctly.     

Access Port Covers for EV Cooling Systems

How to Select the Right Plastic for Your Project

Our expert team will guide you through our EMI shielding and injection molded plastics solutions, discussing their unique properties, strengths, and applications. Whether you're working to reduce weight or reduce cost, we've got you covered. 

Connect with our knowledgeable experts to help you make the best choice for your project. They are ready to answer your specific quests, provide tailored advice and assist you in selecting the perfect plastic for your project. 

How to Choose the Right Plastic

Electrically Conductive Plastic Pellet Materials

Parker Chomerics PREMIER family of materials are electrically conductive thermoplastics for plastic enclosure EMI shielding solutions. The polymer alloys (PC-ABS or PBT-PC) and conductive fillers are engineered for stable electrical, mechanical, and physical performance.

Parker Image

In This Webinar, You Will Learn About:

  • Metal-to-plastic replacement conversion technology
  • Light-weighting, hardware elimination, and elimination of machine operation
  • Design for manufacturability (DFM)
  • Examples of successful automotive metal-to-plastic conversion
  • Key considerations and highlights
  • And much more!

Benefits of Replacing Metal Parts with Plastic

For automotive engineers looking to reduce vehicle weight, metal-to-plastic conversion is a win-win. At the highest level, injection plastic molds are capable of producing multiples of millions of parts required for automotive programs with ease. Typically, a single tool can support a program for its entire life-cycle, meaning you only must go through the cost and design of tooling just once.

In traditional metal fabrication, you have stamping and die casting, both of which require tool refurbishment, at what can amount to a very significant cost. Although injection mold tooling can be relatively expensive, it is not more expensive than die cast tools and/or stamping tools.

Parker Image

Typically, injection molds will last many times longer than metal tooling. Injection mold tooling are also more flexible than other types of tools, allowing you to incorporate many types of features into a part so that no secondary machining, coating and/or forming is required after the molding operation. And depending on the type of plastic material you select; you can realize excellent strength to weight properties.

electrically conductive thermoplastics for plastic enclosure EMI shielding

Explore More Automotive Solutions

Join us in driving the future of the automotive industry. Explore our range of solutions and discover how we can help you build lighter, more efficient, and environmentally friendly vehicles for a sustainable tomorrow.

Need Help Finding the Plastic Solution? Talk to an Expert Engineer Now.

If you need assistance identifying the most suitable product for your application,  speak with one of our expert engineers. Our team is ready to help.

Cooling Innovation for EV Motors – Guaranteed

To perform safely and efficiently, high-torque electric motors require integrated cooling systems that are up to the challenge. Plastic components provide Original Equipment Manufacturers (OEMs) with a low-cost, space-saving solution to this engineering test, and with built-in machine-based process monitoring, they can rest assured that each manufacturing and assembly step is completed thoroughly and correctly.

Electric truck charging station

Empowering Your Business on a Global Scale

Our manufacturing operations span the globe, allowing us to serve you locally no matter where you are. We understand your unique needs and provide personalized solutions that cater to your specific requirements.

Shop link image

EV Onward is Parker's Portfolio of Electrification Solutions

From adhesives and coatings to gaskets and seals, Parker has been providing solutions for decades. We're leading EV advancement with the same quality and expertise our customers have come to expect. 

Parker EV Onward

Can't find what you're looking for? Talk to one of our experts.