Dairy - Bioscience and Water Filtration Division | Parker US
Parker Bioscience Filtration offers products for brewers across the globe

Sterile air filtration products form Parker Bioscience Filtration eliminate airborne spoilage organisms from a number of gas applications throughout dairy production and packaging processes. Dairy plants with their warm, humid environments can provide the ideal conditions and the nutrients for the proliferation of bacteria resulting in ruined product. Parker Bioscience Filtration offers a range of sterile gas filters for all stages of the produciton and packaging process, helping manufacturers reach distant customers by increasing the shelf life of their product and reducing overall dairy waste from bacterial contamination. 

Sterile Gas for Aseptic Packaging

Aseptic packaging ensures that there is no microbial contamination of dairy products post processing, which fundamentally increases the life-time of the product and protects against worse case scenarios such as large scale product recalls. Sterile air and gas filter cartridges provide an aseptic environment in which dairy products may be packaged to avoid microbial contamination.

Sterile Gas for Tank Filtration

During storage, dairy may come into contact with airborne bacteria transmitted via vents on storage tanks. In order to reduce and eliminate the possibility of product contamination, vents on storage tanks can be fitted with sterile filters which inhibit any spoilage organism from entering the tank.

Product Purge

During the production process, dairy products can remain in the pipes. This product is often pushed along by 'flushing' the pipes with air, forcing the product downstream. The introduction of unfiltered compressed air into the process may introduce micro-organisms into the product. To avoid contamination and maintain food safety, this compressed air can be sterile filtered before use within the production process, maintaining the stability of the final product.

Product Mobility

Sterile gas for product mobility is important at aseptic packaging where product delivery to the packaging process can be via an aseptic IBC. In many cases the IBC is top loaded with compressed gas to provide the motive force to drive through process lines and into the aseptic packaging machinery. To protect from product contamination and spoilage from airborne microorganisms, compressed gas used for product mobility should be sterile filtered close to the point-of-use.

Product Aeration / Foaming

Product aeration allows dairies to be creative and innovative with the textures and mouthfeel of mousses, yogurts and cream cheeses. Aeration is being used to produce lighter products with a smooth mouth feel and reduces sugar and fat contents. The compressed air used in the process poses a significant threat of product spoilage through contamination from airborne microorganisms. Parker provide products which can help eliminate this problem.

Steam Filtration

Steam is principally used for pasteurization or system sterilizing duties. However, due to its aggressive nature, steam can contain a high degree of metal fines or physical particulate, which if not removed, could contaminate product contact surfaces or damage valves. Typically, culinary grade steam is a pre-requisite to reduce the risk of the physical hazards present within steam. For steam filtration, this requires 95% removal of particulate greater than 2µm in size.

Food & Beverage Knowledge & Resources

As part of our commitment to sharing and promoting industry best practice, we have created a technical content hub around sterile filtration and microfiltration solutions. Browse our food and beverage related white papers, technical articles, case studies, videos and application notes.

Bioprocessing Knowledge & Resources

Not sure which product you need? Get in touch with one of our specialists.

close up on man hand holding smartphone with futuristic of social media marketing icon for internet network technology and business concept

 

Bioscience N.A. 

Parker Bioscience & Water Filtration
2340 Eastman Ave.
Oxnard, California
93030 United States
Ph: +1 (805) 604-3400
bwf.oxn.support@support.parker.com

 

Bioscience EMEA 

Parker Hannifin Manufacturing Ltd
Durham Road, Birtley
County Durham
DH3 2SF United Kingdom
Ph: +44 (0)191 4105121
befe.birtley.support@support.parker.com

Looking for Watermakers?