Metal Bonding - Assembly & Protection Solutions Division | Parker US
Parker Image

Standard Operating Procedure for Bonding Repair

Identify

Check for OEM repair guidelines in order to determine if the application should be bond only, weld bond or rivet bond and then proceed with the proper Fusor® Standard Operating Procedure.

Prepare

1. Remove the old panel using care not to damage remaining panels.

 

2. Clean any remaining adhesive or sealers from bonding flanges.

 

3. Using new panel as a guide, confirm all bonding flanges are undamaged and mate up with the replacement panel. Make repairs as needed.

 

4. Prepare for the panel installation by having all necessary clamping devices on hand and determine if panel will be 100% bonded or if a butt-joint exists which will require MIG-welding or MIG-brazing.

 

5. Prepare bonding flanges on replacement panel to receive adhesive. 

 

6. Clean all bonding flanges with solvent. 

 

 

Tech Tips:

 

  • Where original panel is spot welded, use a spot weld removal tool to avoid damage to the mating panel.
  •  Refer to OEM repair guidelines before removing any metal coatings (e.g. zinc coatings such as galvanizing). Always completely remove metal coatings leaving a shiny metal surface when using an acrylic adhesive.
  • Follow OEM repair guidelines regarding the removal of e-coat and metal coatings on service parts. When removing coatings only do so in the bond area and avoid creating areas which are uncoated after the repair is complete.
  • Use a quick evaporating solvent, such as acetone or isopropyl alcohol that leaves no residue behind.

Apply

7. Prepare adhesive for application by purging the cartridge and leveling the plungers before installation of the mixing nozzle and running out a bead to ensure a homogeneous mix.

 

8. Apply adhesive to the bonding area.

 

9. Install and clamp the panel in position.

 

10. Release the clamps once the adhesive has reached its handling strength noted on the product label. 

 

 

Tech Tips:

 

  • When using epoxy based adhesives, such as Fusor 208B or Fusor 2098*, always “butter” both bonding flanges first, and then follow up with application of the adhesive bonding bead. When using an acrylic adhesive, such as Fusor 108B, 108BE** or 112B, do not butter the flanges.
  • If any MIG welded, or MIG brazed, joints exist hold the adhesive back 1" (25-mm) from the weld zone.
  • Once contact is made with the adhesive, slide the panel to its final position – do not separate panels.
  • Application of heat to epoxies will accelerate the adhesive if desired for quicker clamp removal.

Finish

11. Before the adhesive begins to cure:

 

  • Tool any adhesive squeeze out (if using an epoxy),
  • Or wipe off completely (if using an acrylic or epoxy).

Read the Full SOP Now

Unlock the essentials of metal bonding with our comprehensive Standard Operating Procedures. Refine your techniques, ensure precision, and strengthen structural integrity by following industry-leading practices. Start your learning journey now!

Parker Image

Questions? Talk with one of our experts.

Call Us at 877-275-5673