Thermal interface materials (TIMs) and adhesives play a critical role in the thermal management of EV charging infrastructure. They help to transfer heat away from the heat-generating components of charging stations, such as the power electronics, charging handles, and the optional battery backup. This helps to ensure that the charging stations operate efficiently and reliably.
The webinar will be of interest to engineers, designers and other professionals who are involved in the development or operation of EV charging infrastructure. We will discuss the different types of TIMs and adhesives that are used in EV charging infrastructure, as well as their applications and benefits. We will also discuss the factors that need to be considered when selecting the right TIM or adhesive for a particular application.