BORÅS, Schweden, 11. November 2022 – Parker Hannifin, the global leader in motion and control technologies, is announcing a set of next-generation pre-compensated load sensing (LS) valves, as part of the VA Series, designed specifically for highly demanding mobile machinery applications.
The market-leading performance of the VA Series mobile directional control valves ensures outstanding maneuverability and robustness, as well as allowing greater flexibility and modularity. These valves are designed and prepared to meet future demands within a range of challenging industries, such as forestry, construction, mining and material handling.
The VA Series is based on Parker’s existing high-end L90LS and K220LS valves that are renowned for their robustness, controllability and flexibility. These next-generation pre-compensated LS valves have been substantially improved to increase modularity and to allow customer efficient solutions. For example, these valves have been designed with a focus on reducing space claim and enhancing mounting possibilities, while also optimizing channels to minimize flow losses.
With a maximum flow to workport of up to 450 l/min, the VA Series follows in the footsteps of the K220LS valve and takes the performance to the next level. The VA Series has been designed and optimized with features such as on-board electronics and readiness for Industry 4.0 or any other future demands regarding IoT and diagnostics. In addition to this, the new valve series also incorporates latest hydraulic features – proportional counter pressure with active refill, warm-up possibilities, plus several other performance-enhancing improvements that herald the dawn of the next generation in mobile directional control valves.
With the VA Series, Parker continues to deliver high-end solutions with function adapted spools and seamless integration of function manifolds specially designed for specific customer needs. With focus on sustainability and energy efficiency from raw material to finished product reducing the total environmental footprint, the VA Series remains true to Parker’s goal of engineering for a better tomorrow.
The VA300 is the first valve of the new series to be released. The next valve in the series, VA450, is set to be launched at the start of 2023.
Learn more about the VA Series at: https://ph.parker.com/gb/en/mobile-directional-contol-valve-va-series
About Pump & Motor Division Europe
Parker Pump & Motor Division Europe (PMDE) constantly strives to find new solutions that can help customers build better and more productive machines. With this mission in mind, PMDE designed the Customer Service Program to supply customers with the right system or component at the right time - no matter whether working directly with Parker, or with one of its premier distributors (www.parker.com/PMDE).
About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century, the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
Anders Johansson
Application Manager
Motion Hydraulic Systems Division Europe, Parker Hannifin
Email: anders.johansson@parker.com
Lisa de Beer
Public Relations EMEA
Parker Hannifin
Phone.: +27 (0)11 961 0700
Email: lisa.debeer@parker.com