Heatric Manufacturing - Division Homepage Template | Parker
Pressure Gauges - Heatric Manufacturing

Heatric manufacturing covers every stage of the production process and includes proprietary diffusion bonding processes, world class high-alloy welding capabilities and on-site fabrication and testing.

Heatric manufacturing produces diffusion bonded heat exchangers in the UK with co-manufacturing partners in Sao Paulo, Brazil to provide local services for our South American customers.

Heatric has extensive manufacturing and testing facilities across our sites and is continually looking for ways to expand its operations.

 

Flow plate manufacturing

The Heatric PCHE manufacturing process begins at the etching stage where stainless steel flow plates are prepared, etched and finished before bonding and final assembly.

At this stage, the etching team complete the following:

  • Plate preparation
  • Plate etching design and film preparation
  • Etched plate production and finishing
  • Quality assurance and checking

 

Diffusion bonding and fabrication

At this stage the diffusion bonding, component sub-assembly, and final assembly of Heatric’s exchangers takes place. The units undergo extensive on-site testing in Heatric’s dedicated radiographic facilities. The Poole manufacturing site features:

  • 20 acre site
  • 25,000m² production facilities across 3 factories
  • Administration
  • Engineering
  • Project management
  • Bonding
  • Assembly
  • Testing

FEATURED VIDEO

Heat Exchanger Construction

Parker Image

Compliance, Health, Safety and the Environment at Heatric

Heatric has a commitment to quality, health, safety and the environment. The company operates an Integrated Management System (IMS) which is accredited to BS EN ISO 9001, ISO 14001 and ISO 45001, and the mechanical design of any PCHE is always in accordance with the design code specified by the customer.

Heatric Heat Exchanger Manufacturing

Need Help?

Can't Find What You're Looking For? Get in Touch With One of Experts