MAN Energy Solutions will supply the ETES heat pump technology to Danish multi-utility company DIN Forsyning. This ground-breaking solution offers a carbon-neutral alternative to traditional fossil fuel power plants, harnessing wind and seawater hydro power to supply energy to approximately 100,000 local inhabitants. The MAN ETES heat pump installation is both the largest sea water heat pump in Denmark and the largest heat pump in the world to use CO2 as a refrigerant.
Adrian Tattersall, General Manager of Meggitt’s Heatric organisation said “We are delighted to be supporting MAN Energy Solutions on such a pioneering and environmentally beneficial project. The contract award demonstrates Heatric’s ability to work closely with our customers to provide innovative technical solutions to support clean energy. Our PCHEs are central to the system and provide the thermal transfer between the innovative CO2 refrigerant loop and the district heating network. This award further supports our ambition to provide optimized heat transfer solutions to the growing Green technology market”.
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
###
Melissa Frink
Manager, Corporate Communications
6035 Parkland Blvd.
Cleveland, OH 44124
216 896 3257